This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Audio In of Beagleboard xM Rev.C is not working

hi all,

                   i have a beagleboard xm rev.c which is ported on to dvsdk 4.01, angstrom linux kernel ver.2.6.32 running on it. 

                   when i record voice in beagleboard using arecord command and play it back i hear only noise and not the voice which was recorded.

                  Headset Mic was used for the recording purpose.

                  voltage level when measured at the audio-in port is found to be 0.02V (both left and right). 

                 optimum level required for voice recording is around 2V-2.2V

                 how do i solve this problem??

 

regards,

shravan