Part Number: AM625
Tool/software:
Greetings,
I am using a custom board (MYIR) based on the AM6254.
I built linux-6.1.y with the custom device tree and booted from the SD card without issue.
However, when I attempt to do the same thing with linux-6.6.y, the device cannot see the SD card.
Waiting for root device PARTUUID=076c4a2a-02...
My thought is that this is related to the device tree - but I don't know why it would change between the kernel revisions.
What troubleshooting steps can I take to diagnose this?