Hello all,
I am facing issues in mounting through nfs.
The output of printenv is as follows and i have kept the board in dhcp mode:
bootdelay=4
baudrate=115200
setboot=setenv bootargs $(bootargs)
bootamd=nboot 0x80700000 0 0x500000;bootm
bootfile=""
setenv=bootargs console=ttyS1,115200n8 noinitrd rw root=/dev/nfs nfsroot=10.17.8.125:/home/mayank/DM36/ipnc/target/filesys,nolock mem=48M ip=dhcp
ip=ddr 10.17.8.125
ethaddr=00:0C:0C:A0:FF:FA
eth=00:0C:0C:A0:07:Ea
bootcmd=nboot 0x80700000 0 0x500000;bootm
nfshost=10.17.1.101
rootpath=/home/mayank/DM368IPNC/ipnc/target/filesys
filesize=1D5610
fileaddr=80700000
serverip=10.17.1.101
ipaddr=10.17.1.102
bootargs=console=ttyS1,115200n8 noinitrd rw ip=10.17.1.102:10.17.1.101::255.255.255.0::eth0:off root=/dev/nfs nfsroot=10.17.1.101:/home/mayank/DM368IPNC/ipnM
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 1.3.4 (Dec 9 2010 - 17:44:14) DM368-IPNC-1.0.1
Environment size: 811/131068 bytes
But after sometime i get the board prompt i get the messages like this:
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
net_get_netmask: ioctl SIOCGIFNETMASK: Cannot asnfs: RPC call returned error 101
sign requested address
nfs: RPC call returned error 101
nfs: RPC call returned error 101
net_get_netmask: ioctl SIOCGIFNETMASK: Cannot assign requested anfs: RPC call returned error 101
ddress
nfs: RPC call returned error 101
net_get_netmask:nfs: RPC call returned error 101
ioctl SIOCGIFNEnfs: RPC call returned error 101
TMASK: Cannot asnfs: RPC call returned error 101
sign requested anfs: RPC call returned error 101
ddress
Error: dnfs: RPC call returned error 101
hcp fail
FileMnnfs: RPC call returned error 101
g: Error Can't cnfs: RPC call returned error 101
reate log file
nfs: RPC call returned error 101
FileMng: Error Cnfs: RPC call returned error 101
an't create systnfs: RPC call returned error 101
em file
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
nfs: RPC call returned error 101
/proc/net/route:nfs: RPC call returned error 101
If in bootargs i chnage from ip = 10.17.1.102:10.17.1.101::255.255.255.0::eth0:off to ip=dhcp my boot gets stuck up at
Sending DHCP requests .... timed out and as a result i am not able to boot in dhcp mode.
Please also find the bootlog for the above scenario as given below:
Loading from NAND 128MiB 3,3V 8-bit, offset 0x500000
Image Name: Linux-2.6.18_pro500-davinci_IPNC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1922512 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.18_pro500-davinci_IPNC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1922512 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.6.0 (root@mayank-laptop) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Thu O1
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM368 IPNC
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x8
PLL0: fixedrate: 24000000, commonrate: 170000000, vpssrate: 340000000
PLL0: vencrate_sd: 75555555, ddrrate: 340000000 mmcsdrate: 48571428
PLL1: armrate: 432000000, voicerate: 20571428, vencrate_hd: 27000000
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists. Total pages: 14336
Kernel command line: console=ttyS1,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=10.17.1.101:/home/mayank/DM368IPNC/ipnc/target/filesys,nolock mem=56M
PID hash table entries: 256 (order: 8, 1024 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 56MB = 56MB total
Memory: 52492KB available (3309K code, 686K data, 184K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
MUX: initialized GPIO20
MUX: initialized I2C_SCL
DM365 IPIPE initialized in Single Shot mode
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
SCSI subsystem initialized
NET: Registered protocol family 2
IP route cache hash table entries: 512 (order: -1, 2048 bytes)
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 2048 bind 1024)
TCP reno registered
***davinci_spi_board_init()!<6>
***davinci_spi_board_init_End(0)!<5>VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Oct 20 2011 16:09:17 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
davinci_ldc initialized
facedetect major#: 252, minor# 0
facedetect driver registered
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Davinci EMAC MII Bus: probed
MAC address is deadbeaf
TI DaVinci EMAC Linux version updated 4.0
netconsole: not configured, aborting
Linux video capture interface: v2.00
vpfe_init
starting ccdc_reset...<7>
End of ccdc_reset...<5>vpfe_probe
Trying to register davinci display video device.
layer=c06b6000,layer->video_dev=c06b6160
Trying to register davinci display video device.
layer=c05d0e00,layer->video_dev=c05d0f60
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
i2c /dev entries driver
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Creating 7 MTD partitions on "nand_davinci.0":
0x00000000-0x00300000 : "bootloader"
0x00300000-0x00500000 : "params"
0x00500000-0x00700000 : "kernel"
0x00700000-0x02700000 : "filesystem"
0x02700000-0x02900000 : "data1"
0x02900000-0x02d00000 : "Calibration"
0x02d00000-0x08000000 : "data2"
nand_davinci nand_davinci.0: hardware revision: 2.3
MUX: initialized SPI0_SCLK
MUX: initialized SPI0_SDO)
dm_spi.0: davinci SPI Controller driver at 0xc4066000 (irq = 42) use_dma=0
musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Peripheral mode controller at c4068000 using DMA, IRQ 12
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: proc
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: dev (254:0)
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as rtc0
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
CQ0093 Voice Codec 0.1
asoc: cq93vc <-> davinci-vcif mapping ok
ALSA device list:
#0: On-chip voice codec (cq93vc)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2000-01-01 06:21:05 (946707665)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
Sending DHCP requests ......
I am sure that there is no issue with my uimage and filesystem.The issue may be network or nfs but
i am not understanding why it is happening and how can i rectify that.
Please suggest solutions for the same.
Regards,
Mayank