This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Accessing PCIe Altera device BAR memory results in unhandled fault



Hi,

We have a DM816x/C6A816x/AM389x Evaluation Module of which we are using the PCIe interface to communicate with a configured Altera Cyclone IV FPGA development board.

During EVM Ubuntu boot, with FPGA card attached,  the following PCIe information is given:

ti816x_pcie: Invoking PCI BIOS...
ti816x_pcie: Setting up Host Controller...
ti816x_pcie: Register base mapped @0xd0820000
ti816x_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 9: assigned [mem 0x20000000-0x21ffffff pref]
pci 0000:00:00.0: BAR 8: assigned [mem 0x22000000-0x220fffff]
pci 0000:01:00.0: BAR 0: assigned [mem 0x20000000-0x21ffffff 64bit pref]
pci 0000:01:00.0: BAR 0: set to [mem 0x20000000-0x21ffffff 64bit pref] (PCI address [0x20000000-0x21ffffff])
pci 0000:01:00.0: BAR 2: assigned [mem 0x22000000-0x2203ffff]
pci 0000:01:00.0: BAR 2: set to [mem 0x22000000-0x2203ffff] (PCI address [0x22000000-0x2203ffff])
pci 0000:01:00.0: BAR 3: assigned [mem 0x22040000-0x2207ffff]
pci 0000:01:00.0: BAR 3: set to [mem 0x22040000-0x2207ffff] (PCI address [0x22040000-0x2207ffff])
pci 0000:00:00.0: PCI bridge to [bus 01-01]
pci 0000:00:00.0:   bridge window [io  disabled]
pci 0000:00:00.0:   bridge window [mem 0x22000000-0x220fffff]
pci 0000:00:00.0:   bridge window [mem 0x20000000-0x21ffffff pref]
PCI: enabling device 0000:00:00.0 (0140 -> 0143)

Note BAR0 is configured 64-bit prefetchable memory (32Mb) and BAR2 configured as 32-bit non-prefetchable memory (256Kb).

Our driver (originally supplied by Altera) then registers, reads the device configuration, scans and maps the bars. The following debugs are given during this stage:

probe(dev = 0xcc826c00, pciid = 0xbf1f87cc)
probe() ape = 0xcb754600
sizeof(struct ape_chdma_table) = 4096.
table_virt = ffc14000, table_bus = 0x        8a91a000.
PCI: enabling device 0000:01:00.0 (0140 -> 0142)
Enabled MSI interrupting.
Using a 64-bit DMA mask.
IRQ pin #1 (0=none, 1=INTA#...4=INTD#).
IRQ line #48.
Succesfully requested IRQ #112 with dev_id 0xcb754600
BAR0 0x20000000-0x21ffffff flags 0x0014220c
BAR2 0x22000000-0x2203ffff flags 0x00040200
BAR[0] mapped at 0xd56d8000 with length 16384(/33554432) flags = 0x0014220c.
BAR[2] mapped at 0xd5780000 with length 262144(/262144) flags = 0x00040200.
fpga_tests()
ptrHeader0 = 0xd56d8000
ptrHeader1 = 0x0
ptrHeader2 = 0xd5780000

We can then read/write BAR0 without any problems e.g.

printk(KERN_INFO "BAR 1 %d = %0llx ", i, ptrHeader0[i++]);

However, when it comes to accessing ANY part of BAR2 e.g.

printk(KERN_INFO "BAR 2 %d = %0llx ", i, ptrHeader2[i++]);

We get the following memory fault:

Unhandled fault: Precise External Abort on non-linefetch (0x1008) at 0xd5780000
Internal error: : 1008 [#1]
last sysfs file: /sys/module/pvrsrvkm/initstate
Modules linked in: altpciechdma(+) bufferclass_ti omaplfb pvrsrvkm TI81xx_hdmi ti81xxfb vpss syslink ipv6
CPU: 0    Not tainted  (2.6.37 #1)
...

We have managed to determine via instrumentation, that BAR2 of the FPGA is never being accessed so assume the the problem is lying somewhere on the Linux side e.g. root complex.  

Does anybody have some idea of what we may be doing wrong? We have looked and re-looked at this but can't find anything.

Many thanks,

Dave

 

  • Dave,

    Can you provide the 'lspci -xvv' dump before and after accessing BAR2? Note that you will need pciutils in the filesystem.

       Hemant

     

  • Hi Hemant,

    Thanks for coming back on this one. Pciutils does not exist on my standard TI EZDSK install. I will attempt to locate and build it for the target.  As soon as I have success I will print the results you requested here.

    Regards,

    Dave

  • OK Hemant here is the requested information.

    Before calling the driver:

    root@dm816x-evm:/home/dave/downloads/pciutils-3.1.8# ./lspci -xvv
    00:00.0 Class 0604: Device 104c:8888 (rev 01)
            Control: I/O+ Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx-
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Latency: 0, Cache Line Size: 64 bytes
            Region 0: Memory at <ignored> (32-bit, non-prefetchable)
            Region 1: Memory at <ignored> (32-bit, prefetchable)
            Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
            Memory behind bridge: 22000000-220fffff
            Prefetchable memory behind bridge: 20000000-21ffffff
            Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
            BridgeCtl: Parity+ SERR- NoISA- VGA- MAbort- >Reset- FastB2B-
                    PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
            Capabilities: [40] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
                    Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [50] MSI: Enable- Count=1/1 Maskable- 64bit+
                    Address: 0000000000000000  Data: 0000
            Capabilities: [70] Express (v2) Root Port (Slot-), MSI 00
                    DevCap: MaxPayload 256 bytes, PhantFunc 0, Latency L0s <64ns, L1 <1us
                            ExtTag- RBE+ FLReset-
                    DevCtl: Report errors: Correctable- Non-Fatal- Fatal- Unsupported-
                            RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                            MaxPayload 128 bytes, MaxReadReq 512 bytes
                    DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr- TransPend-
                    LnkCap: Port #0, Speed 5GT/s, Width x2, ASPM L0s, Latency L0 <2us, L1 <64us
                            ClockPM- Surprise- LLActRep+ BwNot-
                    LnkCtl: ASPM Disabled; RCB 128 bytes Disabled- Retrain- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive+ BWMgmt- ABWMgmt-
                    RootCtl: ErrCorrectable- ErrNon-Fatal- ErrFatal- PMEIntEna- CRSVisible-
                    RootCap: CRSVisible-
                    RootSta: PME ReqID 0000, PMEStatus- PMEPending-
                    DevCap2: Completion Timeout: Range ABCD, TimeoutDis+ ARIFwd-
                    DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis- ARIFwd-
                    LnkCtl2: Target Link Speed: 5GT/s, EnterCompliance- SpeedDis-, Selectable De-emphasis: -6dB
                             Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                             Compliance De-emphasis: -6dB
                    LnkSta2: Current De-emphasis Level: -3.5dB
            Capabilities: [100 v1] Advanced Error Reporting
                    UESta:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UEMsk:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
                    CESta:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr-
                    CEMsk:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr+
                    AERCap: First Error Pointer: 00, GenCap+ CGenEn- ChkCap+ ChkEn-
    00: 4c 10 88 88 47 01 10 00 01 00 04 06 10 00 01 00
    10: 00 00 00 51 08 00 00 80 00 01 01 00 f0 00 00 00
    20: 00 22 00 22 00 20 f0 21 00 00 00 00 00 00 00 00
    30: 00 00 00 00 40 00 00 00 00 00 00 00 30 01 01 00

    01:00.0 Class ff00: Device 1172:0004 (rev 01)
            Subsystem: Device 1172:0004
            Control: I/O- Mem- BusMaster- SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx-
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Interrupt: pin A routed to IRQ 48
            Region 0: Memory at 20000000 (64-bit, prefetchable) [disabled] [size=32M]
            Region 2: Memory at 22000000 (32-bit, non-prefetchable) [disabled] [size=256K]
            Region 3: Memory at 22040000 (32-bit, non-prefetchable) [disabled] [size=256K]
            Capabilities: [50] MSI: Enable- Count=1/4 Maskable- 64bit+
                    Address: 0000000000000000  Data: 0000
            Capabilities: [68] MSI-X: Enable- Count=1 Masked-
                    Vector table: BAR=0 offset=00081800
                    PBA: BAR=7 offset=00001800
            Capabilities: [78] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
                    Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [80] Express (v1) Endpoint, MSI 00
                    DevCap: MaxPayload 256 bytes, PhantFunc 0, Latency L0s <64ns, L1 <1us
                            ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset-
                    DevCtl: Report errors: Correctable- Non-Fatal- Fatal- Unsupported-
                            RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                            MaxPayload 128 bytes, MaxReadReq 512 bytes
                    DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr- TransPend-
                    LnkCap: Port #1, Speed 2.5GT/s, Width x1, ASPM L0s, Latency L0 unlimited, L1 unlimited
                            ClockPM- Surprise- LLActRep- BwNot-
                    LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- Retrain- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
            Capabilities: [100 v1] Virtual Channel
                    Caps:   LPEVC=0 RefClk=100ns PATEntryBits=1
                    Arb:    Fixed- WRR32- WRR64- WRR128-
                    Ctrl:   ArbSelect=Fixed
                    Status: InProgress-
                    VC0:    Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                            Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                            Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                            Status: NegoPending- InProgress-
    00: 72 11 04 00 40 01 10 00 01 00 00 ff 10 00 00 00
    10: 0c 00 00 20 00 00 00 00 00 00 00 22 00 00 04 22
    20: 00 00 00 00 00 00 00 00 00 00 00 00 72 11 04 00
    30: 00 00 00 00 50 00 00 00 00 00 00 00 30 01 00 00


    After calling the driver that caused Unhandled fault: Precise External Abort on non-linefetch (0x1008) at 0xd5780000
    Internal error: : 1008 [#1]...

    root@dm816x-evm:/home/dave/downloads/pciutils-3.1.8# ./lspci -xvv
    00:00.0 Class 0604: Device 104c:8888 (rev 01)
            Control: I/O+ Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx-
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Latency: 0, Cache Line Size: 64 bytes
            Region 0: Memory at <ignored> (32-bit, non-prefetchable)
            Region 1: Memory at <ignored> (32-bit, prefetchable)
            Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
            Memory behind bridge: 22000000-220fffff
            Prefetchable memory behind bridge: 20000000-21ffffff
            Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
            BridgeCtl: Parity+ SERR- NoISA- VGA- MAbort- >Reset- FastB2B-
                    PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
            Capabilities: [40] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
                    Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [50] MSI: Enable- Count=1/1 Maskable- 64bit+
                    Address: 0000000000000000  Data: 0000
            Capabilities: [70] Express (v2) Root Port (Slot-), MSI 00
                    DevCap: MaxPayload 256 bytes, PhantFunc 0, Latency L0s <64ns, L1 <1us
                            ExtTag- RBE+ FLReset-
                    DevCtl: Report errors: Correctable- Non-Fatal- Fatal- Unsupported-
                            RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                            MaxPayload 128 bytes, MaxReadReq 512 bytes
                    DevSta: CorrErr- UncorrErr+ FatalErr- UnsuppReq- AuxPwr- TransPend-
                    LnkCap: Port #0, Speed 5GT/s, Width x2, ASPM L0s, Latency L0 <2us, L1 <64us
                            ClockPM- Surprise- LLActRep+ BwNot-
                    LnkCtl: ASPM Disabled; RCB 128 bytes Disabled- Retrain- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive+ BWMgmt- ABWMgmt-
                    RootCtl: ErrCorrectable- ErrNon-Fatal- ErrFatal- PMEIntEna- CRSVisible-
                    RootCap: CRSVisible-
                    RootSta: PME ReqID 0000, PMEStatus- PMEPending-
                    DevCap2: Completion Timeout: Range ABCD, TimeoutDis+ ARIFwd-
                    DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis- ARIFwd-
                    LnkCtl2: Target Link Speed: 5GT/s, EnterCompliance- SpeedDis-, Selectable De-emphasis: -6dB
                             Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                             Compliance De-emphasis: -6dB
                    LnkSta2: Current De-emphasis Level: -3.5dB
            Capabilities: [100 v1] Advanced Error Reporting
                    UESta:  DLP- SDES- TLP- FCP- CmpltTO+ CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UEMsk:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
                    CESta:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr-
                    CEMsk:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr+
                    AERCap: First Error Pointer: 0e, GenCap+ CGenEn- ChkCap+ ChkEn-
    00: 4c 10 88 88 47 01 10 00 01 00 04 06 10 00 01 00
    10: 00 00 00 51 08 00 00 80 00 01 01 00 f0 00 00 00
    20: 00 22 00 22 00 20 f0 21 00 00 00 00 00 00 00 00
    30: 00 00 00 00 40 00 00 00 00 00 00 00 30 01 01 00

    01:00.0 Class ff00: Device 1172:0004 (rev 01)
            Subsystem: Device 1172:0004
            Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx+
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Latency: 0, Cache Line Size: 64 bytes
            Interrupt: pin A routed to IRQ 368
            Region 0: Memory at 20000000 (64-bit, prefetchable) [size=32M]
            Region 2: Memory at 22000000 (32-bit, non-prefetchable) [size=256K]
            Region 3: Memory at 22040000 (32-bit, non-prefetchable) [size=256K]
            Capabilities: [50] MSI: Enable+ Count=1/4 Maskable- 64bit+
                    Address: 0000000051000054  Data: 0000
            Capabilities: [68] MSI-X: Enable- Count=1 Masked-
                    Vector table: BAR=0 offset=00081800
                    PBA: BAR=7 offset=00001800
            Capabilities: [78] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
                    Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [80] Express (v1) Endpoint, MSI 00
                    DevCap: MaxPayload 256 bytes, PhantFunc 0, Latency L0s <64ns, L1 <1us
                            ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset-
                    DevCtl: Report errors: Correctable- Non-Fatal- Fatal- Unsupported-
                            RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                            MaxPayload 128 bytes, MaxReadReq 512 bytes
                    DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr- TransPend-
                    LnkCap: Port #1, Speed 2.5GT/s, Width x1, ASPM L0s, Latency L0 unlimited, L1 unlimited
                            ClockPM- Surprise- LLActRep- BwNot-
                    LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- Retrain- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
            Capabilities: [100 v1] Virtual Channel
                    Caps:   LPEVC=0 RefClk=100ns PATEntryBits=1
                    Arb:    Fixed- WRR32- WRR64- WRR128-
                    Ctrl:   ArbSelect=Fixed
                    Status: InProgress-
                    VC0:    Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                            Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                            Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                            Status: NegoPending- InProgress-
            Kernel driver in use: altpciechdma
    00: 72 11 04 00 46 05 10 00 01 00 00 ff 10 00 00 00
    10: 0c 00 00 20 00 00 00 00 00 00 00 22 00 00 04 22
    20: 00 00 00 00 00 00 00 00 00 00 00 00 72 11 04 00
    30: 00 00 00 00 50 00 00 00 00 00 00 00 30 01 00 00

    Dave

     

     

     

     

  • I have also checked the following similar issues

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/98131.aspx?PageIndex=2

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/105195.aspx

    and have confirmed the recommended patches were already installed on my system.

    Any ideas?

  • Dave,

    From the difference in lspci output, it seems the DM816x didn't receive the completion for the read request it sent out (completion timeout status is high).

    But as you have already confirmed, the FPGA has not received the read request so it is not going to send the completion. This also confirms the reason there is not corresponding error in FPGA PCIe registers.

    The reason could be :

    The address for read from DM816x is different (possible reason - outbound configuraiton of DM816x being wrong) than that configured in BAR2 of FPGA, thus FPGA would not take that request.

    Though I find it unlikely since BAR0 access works fine, can you provide the register dumpt of 4KB region from 0x51000000?

    Another option is to first force BAR0 on FPGA as 32-bit only and see if all address ranges are accessible since the DM816x RC driver only sets up 32-bit addressing.

       Hemant

     

  • Hi,

    I am facing a similar issue with my setup.. Please help me to resolve the same.

    We have a DM816x/C6A816x/AM389x Evaluation Module of which we are using the PCIe interface to communicate with a \

    configured Altera Arria II GX  FPGA development board.

    During EVM Ubuntu boot, with FPGA card attached,  the following PCIe information is given:

    ti816x_pcie: Invoking PCI BIOS...
    ti816x_pcie: Setting up Host Controller...
    ti816x_pcie: Register base mapped @0xd0820000
    ti816x_pcie: Starting PCI scan...
    PCI: bus0: Fast back to back transfers disabled
    PCI: bus1: Fast back to back transfers disabled
    pci 0000:00:00.0: BAR 9: assigned [mem 0x20000000-0x21ffffff pref]
    pci 0000:00:00.0: BAR 8: assigned [mem 0x22000000-0x220fffff]
    pci 0000:01:00.0: BAR 0: assigned [mem 0x20000000-0x200fffff]
    pci 0000:01:00.0: BAR 0: set to [mem 0x20000000-0x200fffff] (PCI address [0x20000000-0x200fffff])
    pci 0000:00:00.0: PCI bridge to [bus 01-01]
    pci 0000:00:00.0:   bridge window [io  disabled]
    pci 0000:00:00.0:   bridge window [mem 0x22000000-0x220fffff]
    pci 0000:00:00.0:   bridge window [mem 0x20000000-0x21ffffff pref]
    PCI: enabling device 0000:00:00.0 (0140 -> 0143)

    Note only One memory BAR is configured in FPGA.  BAR0 is configured 32-bit non-prefetchable memory (1Mb)

    Our driver then registers, reads the device configuration, scans and maps the bars. The following debugs are given during this stage:

    probe() ape = 0xcb754600
    PCI: enabling device 0000:01:00.0 (0140 -> 0142)
    Enabled MSI interrupting.
    Using a 64-bit DMA mask.
    IRQ pin #1 (0=none, 1=INTA#...4=INTD#).
    IRQ line #48.
    Succesfully requested IRQ #112 with dev_id 0xcb754600
    BAR0 0x20000000-0x200fffff flags 0x00040200
    BAR[0] mapped at 0xd5780000 with length 1048576 flags = 0x00040200.
    fpga_tests()

    when it comes to accessing ANY part of BAR0 e.g.

    printk(KERN_INFO "BAR 0 %d = %0llx ", i, ptrMem[i++]);

    We get the following memory fault:

    Unhandled fault: Precise External Abort on non-linefetch (0x1008) at 0xd5780000
    Internal error: : 1008 [#1]
    last sysfs file: /sys/module/pvrsrvkm/initstate
    Modules linked in: altpciechdma(+) bufferclass_ti omaplfb pvrsrvkm TI81xx_hdmi ti81xxfb vpss syslink ipv6
    CPU: 0    Not tainted  (2.6.37 #1)

    I tried disabling the MSI interrupt support in the Kernel configuration and in the PCIe device driver, But that didn't help me out.

    As per the solution provided , i have verified the Address writtem to the FPGA configuation space BAR0 register by the processor is same

    as the address assigned for the PCIe outbound memory access (ie. 0x2000000 ). Here is the lspci command output after loading the pcie device driver

    and access failure to the FPGA memory window. I am getting the same completion timeout error (CmpltTO+) in the RC error status Register.

    root@vp4000:~/pcie_fpga# ./lspci -xvvv
    00:00.0 Class 0604: Device 104c:8888 (rev 01)
        Control: I/O+ Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx-
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Latency: 0, Cache Line Size: 64 bytes
            Region 0: Memory at <red> (32-bit, Region 1: Memory at <ignored>(32-bit, prefetchable)
            Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
            I/O behind bridge: 0000f000-00000fff     
            Memory behind bridge: 20000000-200fffff   Prefetchable memory behind bridge: fff00000-000fffff
            Secondary status : 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
            BridgeCtl: Parity+ SERR- NoISA-eset- FastB2B- PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
            Capabilities: [40] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
                    Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [50] MSI: Enable- Count=1/1 Maskable- 64bit+
                    Address: 0000000000000000  Data: 0000
            Capabilities: [70] Express (v2) Root Port (Slot-), MSI 00
                    DevCap: MaxPayload 256 bytes, PhantFunc 0, Latency L0s <64ns, L1 <1us
                            ExtTag- RBE+ FLReset-
                    DevCtl: Report errors: Correctable- Non-Fatal- Fatal- Unsupported-
                            RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                            MaxPayload 128 bytes, MaxReadReq 512 bytes
                    DevSta: CorrErr- UncorrErr+ FatalErr- UnsuppReq- AuxPwr- TransPend-
                    LnkCap: Port #0, Speed 5GT/s, Width x2, ASPM L0s, Latency L0 <2us, L1 <64us
                            ClockPM- Surprise- LLActRep+ BwNot-
                    LnkCtl: ASPM Disabled; RCB 128 bytes Disabled- Retrain- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive+ BWMgmt- ABWMgmt-
                    RootCtl: ErrCorrectable- ErrNon-Fatal- ErrFatal- PMEIntEna- CRSVisible-
                    RootCap: CRSVisible-
                    RootSta: PME ReqID 0000, PMEStatus- PMEPending-
                    DevCap2: Completion Timeout: Range ABCD, TimeoutDis+ ARIFwd-
                    DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis- ARIFwd-
                    LnkCtl2: Target Link Speed: 5GT/s, EnterCompliance- SpeedDis-, Selectable De-emphasis: -6dB
                             Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                             Compliance De-emphasis: -6dB
                    LnkSta2: Current De-emphasis Level: -3.5dB
            Capabilities: [100 v1] Advanced Error Reporting
                    UESta:  DLP- SDES- TLP- FCP- CmpltTO+ CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UEMsk:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
                    CESta:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr-
                    CEMsk:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr+
                    AERCap: First Error Pointer: 0e, GenCap+ CGenEn- ChkCap+ ChkEn-
    00: 4c 10 88 88 47 01 10 00 01 00 04 06 10 00 01 00
    10: 00 00 00 51 08 00 00 80 00 01 01 00 f0 00 00 00
    20: 00 20 00 20 f0 ff 00 00 00 00 00 00 00 00 00 00
    30: 00 00 00 00 40 00 00 00 00 00 00 00 30 01 01 00

    01:00.0 Class ff00: Device 1172:0004 (rev 01)
            Subsystem: Device 1172:0004
            Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx-
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Latency: 0, Cache Line Size: 64 bytes
            Interrupt: pin A routed to IRQ 48
            Region 0: Memory at 20000000 (32-bit, non-prefetchable) [size=1M]
            Capabilities: [50] MSI: Enable- Count=1/4 Maskable- 64bit+
                    Address: 0000000000000000  Data: 0000
            Capabilities: [78] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
                    Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [80] Express (v1) Endpoint, MSI 00
                    DevCap: MaxPayload 128 bytes, PhantFunc 0, Latency L0s <64ns, L1 <1us
                            ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset-
                    DevCtl: Report errors: Correctable- Non-Fatal- Fatal- Unsupported-
                            RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                            MaxPayload 128 bytes, MaxReadReq 512 bytes
                    DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr- TransPend-
                    LnkCap: Port #1, Speed 2.5GT/s, Width x1, ASPM L0s, Latency L0 unlimited, L1 unlimited
                            ClockPM- Surprise- LLActRep- BwNot-
                    LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- Retrain- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
            Capabilities: [100 v1] Virtual Channel
                    Caps:   LPEVC=0 RefClk=100ns PATEntryBits=1
                    Arb:    Fixed- WRR32- WRR64- WRR128-
                    Ctrl:   ArbSelect=Fixed
                    Status: InProgress-
                    VC0:    Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                            Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                            Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                            Status: NegoPending- InProgress-
            Kernel driver in use: pcieFpga
    00: 72 11 04 00 46 01 10 00 01 00 00 ff 10 00 00 00
    10: 00 00 00 20 00 00 00 00 00 00 00 00 00 00 00 00
    20: 00 00 00 00 00 00 00 00 00 00 00 00 72 11 04 00
    30: 00 00 00 00 50 00 00 00 00 00 00 00 30 01 00 00

    Please Help me and give some Suggestions to resolve this issue.

    Appreciate your reply....

    Thanks,

    Ansa Ahammed

  • NOTE: Following up above (immediate post before this) issue on http://e2e.ti.com/support/embedded/linux/f/354/t/162993.aspx#594431

       Hemant