Other Parts Discussed in Thread: OMAP-L138, TPS65070, OMAPL138
Hi,
We are using OMAP-L138 SOM from LogicPD.
In our desing we are using Touch screen which is connected to PMIC.
The observation what we have made is when the system is operating from a 3.7V battery touch pressure value read from ADRESULT_1 and ADRESULT_2 shows a value of 0x3FF always even if we do not touch on screen.
When the system is operating with DC 5.0V volts this issue is not observed.
We are following the same circuitry for Touch Screen as there in EVM.
Please suggest how we can debug?
Regards,
GSR