Part Number: AM5716
Tool/software:
Hi:
I noticed that in the document:
"The pre-built TF-A binary should be packaged in TI Processor SDK: <path-to-processor-sdk>/board-support/prebuilt-images/<optional-build-machine-name>/bl31.bin. Use this binary since it has been tested with TI Processor SDK."
"The OP-TEE binary (bl32.bin/tee-pager_v2.bin) is bundled into tispl.bin and the following are the instructions to build:"
that means am5716 supports tf-a and optee, but I just not found bl31.bin(tf-a) and tispl.bin or bl32.bin/tee-pager_v2.bin in the released SDK 9
so I want to confirm the following:
1 Does AM5716 support tf-a and optee in SDK 6.3 / SDK 9 ? If so , is it restrict on only some of 5716 series or all 5716 series support this feature ?
2 is there a test on Ti EVM board as mentioned in the document listed above ?
3 Does AM5716 support arm trust-zone?
thanks