Part Number: J721S2XSOMXEVM
Tool/software:
Hi Ti Expert,
We encountered intermittent memory issues while running the APP, as shown in the attached file.
Consequently, we ran memtester, and the result indicates an issue with the Block Sequential test.
How should we handle this situation?
Should we consider sending the board for repair?
Best Regards,
Hyeonseong.
root@j721s2-evm:~# [ 1428.249398] Unable to handle kernel paging request at virtual address ffff800b7e190220
[ 1428.249865] Unable to handle kernel paging request at virtual address ffff1800080539ec
[ 1428.257330] Kernel panic - not syncing: stack-protector: Kernel stack is corrupted in: console_unlock+0x20c/0x210
[ 1428.257334] SMP: stopping secondary CPUs
[ 1428.265204] Mem abort info:
[ 1428.275437] ESR = 0x0000000086000004
[ 1428.279344] EC = 0x21: IABT (current EL), IL = 32 bits
[ 1428.282125] SET = 0, FnV = 0
[ 1428.285858] EA = 0, S1PTW = 0
[ 1428.291151] FSC = 0x04: level 0 translation fault
[ 1428.294192] swapper pgtable: 4k pages, 48-bit VAs, pgdp=000000008303b000
[ 1428.297320] [ffff1800080539ec] pgd=0000000000000000, p4d=0000000000000000
[ 1428.315628] Internal error: Oops: 0000000086000004 [#1] PREEMPT SMP
[ 1428.321876] Modules linked in: overlay cfg80211 bluetooth ecdh_generic ecc rfkill cryptodev(O) peak_usb can_raw can panel_edp ti_am335x_adc kfifo_buf rpmsg_ctrl rpmsg_char omap_rng cdns3 cdns_usb_common crct10dif_ce display_connector phy_can_transceiver ti_k3_r5_remoteproc wave5 ti_sn65dsi86 videobuf2_dma_contig videobuf2_memops v4l2_mem2mem videobuf2_v4l2 videobuf2_common cdns_mhdp8546 drm_dp_aux_bus ti_am335x_tscadc videodev pvrsrvkm(O) drm_display_helper ti_k3_dsp_remoteproc virtio_rpmsg_bus rpmsg_ns ti_k3_common tidss drm_dma_helper drm_kms_helper mc sa2ul cfbfillrect syscopyarea cfbimgblt sysfillrect sysimgblt fb_sys_fops cfbcopyarea cdns_dphy_rx cdns3_ti optee_rng cdns_dphy m_can_platform m_can can_dev pwm_tiehrpwm rng_core fuse drm drm_panel_orientation_quirks ipv6
[ 1428.390193] CPU: 0 PID: 1054 Comm: sv_vx_app_aptiv Not tainted 6.1.33-g8f7f371be2 #1
[ 1428.397917] Hardware name: Texas Instruments J721S2 EVM (DT)
[ 1428.403558] pstate: 400000c5 (nZcv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 1428.410500] pc : 0xffff1800080539ec
[ 1428.413976] lr : 0xffff1800080539ec
[ 1428.417450] sp : ffff80000b4c3c80
[ 1428.420749] x29: ffff10000b4c3980 x28: ffff000835759c80 x27: ffff00082d92fbe0
[ 1428.427866] x26: 0000000000000002 x25: 0000000000000055 x24: ffff00000b4c2368
[ 1428.434983] x23: 000080000000000a x22: ffff000835759c50 x21: 0000900000000000
[ 1428.442100] x20: ffff80083575f280 x19: 0000b0000000bc0b x18: ffff80000b4c3d68
[ 1428.449218] x17: 0000000000000000 x16: ffff800008da5e10 x15: 0000000000000000
[ 1428.456334] x14: ffff000836dbdc0c x13: 1fffe00106db7b81 x12: ffff80000b4c3d68
[ 1428.463450] x11: 0000000000000000 x10: ffff000836dbdc08 x9 : 0000000000000001
[ 1428.470567] x8 : 0000000000000001 x7 : 0000000000000090 x6 : 0000000000000250
[ 1428.477685] x5 : ffffffffffffd8f8 x4 : 0000000000000000 x3 : ffffffffffffffff
[ 1428.484801] x2 : ffff800b750a6000 x1 : 0000000000000000 x0 : ffff00082e4a73c0
[ 1428.491920] Call trace:
[ 1428.494354] 0xffff1800080539ec
[ 1428.497485] Code: bad PC value
[ 1428.500525] ---[ end trace 0000000000000000 ]---
[ 1428.505126] note: sv_vx_app_aptiv[1054] exited with irqs disabled
[ 1429.324837] SMP: failed to stop secondary CPUs 0-1
[ 1429.329619] Kernel Offset: disabled
[ 1429.333091] CPU features: 0x20000,20028084,0000420b
[ 1429.337952] Memory Limit: none
[ 1429.340994] ---[ end Kernel panic - not syncing: s-ack}prooector: eernul s ack`is uorrupte: inn coosolm_un+ock;0x2xc/0x210 ]---
root@j721s2-evm:~# [ 1428.249398] Unable to handle kernel paging request at virtual address ffff800b7e190220
[ 1428.249865] Unable to handle kernel paging request at virtual address ffff1800080539ec
[ 1428.257330] Kernel panic - not syncing: stack-protector: Kernel stack is corrupted in: console_unlock+0x20c/0x210
[ 1428.257334] SMP: stopping secondary CPUs
[ 1428.265204] Mem abort info:
[ 1428.275437] ESR = 0x0000000086000004
[ 1428.279344] EC = 0x21: IABT (current EL), IL = 32 bits
[ 1428.282125] SET = 0, FnV = 0
[ 1428.285858] EA = 0, S1PTW = 0
[ 1428.291151] FSC = 0x04: level 0 translation fault
[ 1428.294192] swapper pgtable: 4k pages, 48-bit VAs, pgdp=000000008303b000
[ 1428.297320] [ffff1800080539ec] pgd=0000000000000000, p4d=0000000000000000
[ 1428.315628] Internal error: Oops: 0000000086000004 [#1] PREEMPT SMP
[ 1428.321876] Modules linked in: overlay cfg80211 bluetooth ecdh_generic ecc rfkill cryptodev(O) peak_usb can_raw can panel_edp ti_am335x_adc kfifo_buf rpmsg_ctrl rpmsg_char omap_rng cdns3 cdns_usb_common crct10dif_ce display_connector phy_can_transceiver ti_k3_r5_remoteproc wave5 ti_sn65dsi86 videobuf2_dma_contig videobuf2_memops v4l2_mem2mem videobuf2_v4l2 videobuf2_common cdns_mhdp8546 drm_dp_aux_bus ti_am335x_tscadc videodev pvrsrvkm(O) drm_display_helper ti_k3_dsp_remoteproc virtio_rpmsg_bus rpmsg_ns ti_k3_common tidss drm_dma_helper drm_kms_helper mc sa2ul cfbfillrect syscopyarea cfbimgblt sysfillrect sysimgblt fb_sys_fops cfbcopyarea cdns_dphy_rx cdns3_ti optee_rng cdns_dphy m_can_platform m_can can_dev pwm_tiehrpwm rng_core fuse drm drm_panel_orientation_quirks ipv6
[ 1428.390193] CPU: 0 PID: 1054 Comm: sv_vx_app_aptiv Not tainted 6.1.33-g8f7f371be2 #1
[ 1428.397917] Hardware name: Texas Instruments J721S2 EVM (DT)
[ 1428.403558] pstate: 400000c5 (nZcv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 1428.410500] pc : 0xffff1800080539ec
[ 1428.413976] lr : 0xffff1800080539ec
[ 1428.417450] sp : ffff80000b4c3c80
[ 1428.420749] x29: ffff10000b4c3980 x28: ffff000835759c80 x27: ffff00082d92fbe0
[ 1428.427866] x26: 0000000000000002 x25: 0000000000000055 x24: ffff00000b4c2368
[ 1428.434983] x23: 000080000000000a x22: ffff000835759c50 x21: 0000900000000000
[ 1428.442100] x20: ffff80083575f280 x19: 0000b0000000bc0b x18: ffff80000b4c3d68
[ 1428.449218] x17: 0000000000000000 x16: ffff800008da5e10 x15: 0000000000000000
[ 1428.456334] x14: ffff000836dbdc0c x13: 1fffe00106db7b81 x12: ffff80000b4c3d68
[ 1428.463450] x11: 0000000000000000 x10: ffff000836dbdc08 x9 : 0000000000000001
[ 1428.470567] x8 : 0000000000000001 x7 : 0000000000000090 x6 : 0000000000000250
[ 1428.477685] x5 : ffffffffffffd8f8 x4 : 0000000000000000 x3 : ffffffffffffffff
[ 1428.484801] x2 : ffff800b750a6000 x1 : 0000000000000000 x0 : ffff00082e4a73c0
[ 1428.491920] Call trace:
[ 1428.494354] 0xffff1800080539ec
[ 1428.497485] Code: bad PC value
[ 1428.500525] ---[ end trace 0000000000000000 ]---
[ 1428.505126] note: sv_vx_app_aptiv[1054] exited with irqs disabled
[ 1429.324837] SMP: failed to stop secondary CPUs 0-1
[ 1429.329619] Kernel Offset: disabled
[ 1429.333091] CPU features: 0x20000,20028084,0000420b
[ 1429.337952] Memory Limit: none
[ 1429.340994] ---[ end Kernel panic - not syncing: s-ack}prooector: eernul s ack`is uorrupte: inn coosolm_un+ock;0x2xc/0x210 ]---
login as: root
root@10.0.50.100's password:
# cd /jffs2/
# date && ./memtester 900M
Thu Jul 14 07:45:55 UTC 2022
memtester version 4.3.0 (32-bit)
Copyright (C) 2001-2012 Charles Cazabon.
Licensed under the GNU General Public License version 2 (only).
pagesize is 4096
pagesizemask is 0xfffff000
want 900MB (943718400 bytes)
got 900MB (943718400 bytes), trying mlock ...locked.
Loop 1:
Stuck Address : testing 11FAILURE: possible bad address line at offset 0x0f586000.
Skipping to next test...
Random Value : ok
Compare XOR : ok
Compare SUB : ok
Compare MUL : ok
Compare DIV : ok
Compare OR : ok
Compare AND : ok
Sequential Increment: ok
Solid Bits : testing 3FAILURE: 0xff00ff00 != 0x00000000 at offset 0x03ee6010.
FAILURE: 0x00ff00ff != 0xffffffff at offset 0x03ee6014.
FAILURE: 0xff00ff00 != 0x00000000 at offset 0x03ee6018.
Block Sequential : setting 0
Hi TI expert,
We use memtester to test some boards failed.