Tool/software:
Hi, TI expert!
I have a development environment for am6234, with our own evaluation board.
The software SDK version is PROCESSOR-SDK-LINUX-RT-AM62X-08.06.00.42.
May I ask if it is possible to use the serial port of A53 core in R5 core?
For example, I want to run the firmware generated by compiling the MCU SDK in the R5 core, using the main_uart0 serial port of the A53 core in the firmware,as shown in the above figure.
If possible, where can I find the corresponding instructions?
Regards,
Li