This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM69A: AM69A

Part Number: PROCESSOR-SDK-AM69A
Other Parts Discussed in Thread: AM69A

Tool/software:

I am using AM69A EVK board. I am able to run python code from command prompt. The issue i am facing is that when i want to stack 4 camera one below the other . I am not able to set. Other concern is when I run . one row of leveler such as mpu,mcu2_0,c7x_1 and so on. how to remove that to make space. 

In the GUI main screen. 5 button such as Image Classification, object detection and etc how can I stream one came in one button and in second button all 4 cameras at a single time and change the names of the button using debug inside /opt/edgeai-gst-app. Kindly provide solution ASAP.

To run ./apps_python/app_edgeai.py configs/imx219_cam_example.yaml in which file should I place. And for button how to place these

Thanks In advance.