Hi
we are facing system process CPU load is 0% issue, is there anybody can help me. thanks.
DVSDK: v2_18
codec: 02.00.00.09
platform: DM365
encode_stream and wis_streamer process are running in our system. in most of cases, without video stream, encode_stream cpu load is around 20%, but after long-run more than 1 hour, encode_stream cpu load drop down 0%, and other process working fine.