This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM625 / AM623 / AM620-Q1 / AM625-Q1 / AM625SIP / AM62A / AM62D-Q1 / AM62P Custom board hardware design – Partial IO LPM support

Part Number: AM625

Tool/software:

Hi TI Experts,

Could you guide me on testing Partial IO LPM using the SK for UART or USB 

  • Hi Board designers, 

    Refer below recommendations for AM62A SK hardware changes to testing Partial IO LPM 

    USB 

    The USBx_DRVVBUS used to enable the USB power switch has an internal pulldown enabled during reset and after reset.

    In the SK, an external pullup is provided. This needs to be enabled.

    In any of the SK if an external pullup or pulldown is provided, both of these pulls should be made DNI.

    UART 

    The below document describes the changes to be made

    Partialio_LPM_Wakeup.pdf

    Pad Configuration 

    Refer Bit-29

    Additional references

    3.3.5. Low Power Modes — Processor SDK AM62x Documentation

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Generation of VDD_CANUART supply

    Deriving VDDSHV_CANUART from VCC_3V3_MAIN

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Refer below  for Partial IO mode functionality:


    The Partial IO circuits will be disabled the first time power is applied to the processor. When the Partial IO circuits are disable, the MCU_PORz signal will propagate to these circuits. The MCU_PORz signal is blocked from these circuits after software enables the Partial IO functionality (circuits) and configures the processor to monitor wake-up inputs. This is necessary since the MCU_PORz signal will be asserted by the PMIC when it begins the power down sequence associated with the other processor power rails.

    Regards,

    Sreenivasa