Hi TI team,
Pls help me to find what kind of color graphic LCD module which is suitable with OMAP-L317.
Thanks and Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI team,
Pls help me to find what kind of color graphic LCD module which is suitable with OMAP-L317.
Thanks and Best Regards.
Hello Nquyen,
Integrated LCD Controller of OMAP-L137 supports upto 1024 x 1024 x 16 bit color.
The OMAP-L137 has a built-in LCD controller supporting both synchronous (raster-type) and asynchronous (memory-mapped) panels.
The synchronous (raster) module supports STN, color STN, and TFT panels at a resolution of up to 1024 x 1024 x 16-bit color.
Within this range & according to your application can use the following types of standard available GLCDs
1. WQVGA (480x272) (Size 4.3” ) Widescreen, color, transmissive.
2. QVGA (320x240) (Size 3.6") Landscape, color, transmissive w/HRTFT ASIC
3. VGA (640x480) ( Size 6.4” ) Landscape, color, transmissive
Regards
Abhijit