Other Parts Discussed in Thread: OMAP3530
hi,
am working on devkit 8000 (OMAP 3530 ), there are two chip selects, CS0 and CS1. the total physical address provided by OMAP3530 is 1GB, and the address range is given below (according to the OAMP3530 TRM)
CS0 – 0x8000 0000(starting) ---- 0x9FFF FFFF(ending) total= 512MB and
CS1 – 0xA000 0000 (programmable starting) -----0xBFFF FFFF (ending) total =512MB.
so from above information, i can connect 2 lpddr with 512 MB of each.
is it possible to connect 1GB of lpddr to each chip select so i can interface 2GB of SDRAM ?. if so please help me how to do that, any configuration setting or changes in the board itself..
thanks and regards
Babu. N. Reddy