I'm using an am/dm37x Evaluation Module with Linux (angstrom) sd card coming with the board.
When I connect an usb device (keyboard/mouse) into the usb port I get this error on console trace:
hub 2-0:1.0: Cannot enable port 2. Maybe the USB cable is bad?
hub 2-0:1.0: Cannot enable port 2. Maybe the USB cable is bad?
hub 2-0:1.0: Cannot enable port 2. Maybe the USB cable is bad?
hub 2-0:1.0: unable to enumerate USB device on port 2
and the device is unusable.
I built an angstrom image on the Narcissus web site with this configurartion:
Machine: dm37x-evm
Image name: firefox-inside-dm37x-evm
Image type: tgz
Additional Packages:
angstrom-task-gnome
angstrom-uboot-scripts
bash-sh
fennec
firefox
gecko-mediaplayer-firefox-hack
initscripts
shadow
sysvinit
sysvinit-pidof
u-boot
x-load
and I got the same error:
hub 2-0:1.0: Cannot enable port 2. Maybe the USB cable is bad?
hub 2-0:1.0: Cannot enable port 2. Maybe the USB cable is bad?
hub 2-0:1.0: unable to enumerate USB device on port 2.
Our goal is to test fennex/firefox web browser include into angstrom on the evaluation board.
Please suggest us how to solve this hung.
Thanks in advance