Other Parts Discussed in Thread: OMAP-L138, TPS65070, OMAPL138
Hi,
We did some changes to the existing EVM to be operated from a 3.7V 3500mAh Li-Ion battery.
When we execute Touch Level Zero code from CCS what we had observed is Pressure value always shows a value of 0x3FF.
Because of that it doesn't enter into if condition which checks for the TOUCH_HOLD_LIMIT value.
Please suggest what could be the possible reason for this?
Regards,
GSR