I am Guy Shwartz from DVTEL.
I aqm working on DM6437.
I am integrating H264 encoder version 1.12.00 on CCSTUDIO 3.3, DSP bios 5.31.08, CGTOOLS 6.0.8.
All initialization procedures are working properly.
When calling the process function to do the actual encoding I am getting the following error code: 0x8400 which means unsuficient data size.
My question is what can cause this problem and how to solve it?
Also, I could not find a test application that uses this H264 encoder in the DVSDK dowloaded from TI web site. Can you please direct me to such test application.
Thanks alot,
Guy.