Part Number: TDA4VH-Q1
Tool/software:
Hello,
Regarding my previous post (of which I'm hoping "ask a related question" button creating a link) I have updated the flattening process by including batch dimension inside the flattened spatial dimensions. The quantization process is now producing output detections and projected features turned to be non zero. But...
Now the compilation process fails at Memory Planning portion without giving any hints on how to solve it. So can someone help me about what this error is and how to fix it?
For the record, TIDL version 10.00.04, 8 bit and 16 bit quantization gives the same error.
------------------ Fixed-point Calibration Iteration [2 / 2]: ------------------
==================== [Quantization & Calibration Completed] ====================
========================== [Memory Planning Started] ==========================
------------------------- Network Compiler Traces ------------------------------
Successful Memory Allocation
Floating point exception (core dumped)
[TIDL Import] FATAL ERROR: Network Compiler failed to execute - Memory planning failed with return code - 34816 -- [tidl_import_core.cpp, 1002]
[TIDL Import] Aborting
Process finished with exit code 1