Hello,
Reading the SPI TRM for DM8xx, chapter 1.2.4.1, I see the following sentence:
"In slave mode, enabling a channel that is not channel 0 has no effect. Only channel 0 can be enabled."
Does that mean that SPI1 or SPI2 cannot be configured as SPI slave? Or does channel 0 not correspond to SPI0? Thanks and best regards, René