This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMVA2 IPNC 2.6 Alignment trap ERROR



Hi all,

         I have a problem in the DMVA2 IPNC 2.6, the BUG print as follow:

                       TEST DMVA FRATE=10, DETFQ=2, EVTRECEN=1
                       DMVA > IMD:zone 0 - minX = 13,maxX = 49,minY = 43,maxY = 96
                       DMVA > IMD:zone 1 - minX = 3,maxX = 59,minY = 4,maxY = 34

                       > DMVAL: Library framework reset.
                        > DMVAL: Intelligent Motion Detection installed.
                       > DMVAL: Initialized library applications.

                        > DMVA APP: Setting up DMVA-IMD parameters...
                        > DMVA APP: DONE setting up DMVA-IMD parameters...

                        Received New MAIN Parameters

                        ----------------------------
                       queue id:32769
                       queue id:32769
                        Alignment trap: av_server.out (885) PC=0x0005d328 Instr=0xe1d030b2 Address=0x00000001 FSR 0x001

          what's the problem of that?

thanks and regards.