Part Number: SK-TDA4VM
Tool/software:
Hi TI team,
I'm working on converting the custom onyx model using edgeai-tools (09_01_07_00). During the conversion process, I encountered the following issue: Instead of 6 outputs, the resulting model only displays 4. The situation is similar for the two missing outputs: the layer's output should be the output of the model, but it's also passed as input further to the other layers. Note that I get no warnings during compilation regardless of the debug level.
Kind regards,
Aleksandar.