This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VC33 timer0 not operating as expected

Operation writes and reads to timer 1 work correctly, but when writing to timer 0 the timer doesn't reset or count.  This has been verified on three different boards so it's not a bad device.  Even the most basic function of writing 11 (x2c0) to the timer reset and hold which should clear  the counter and start it ticking works on timer 1 but not on timer 0.  Attached is a list of read write operations to timer 1 and timer 0 that also don't work with timer 0 but do for timer 1.

 

Any suggestion on what may be wrong would be appreciated.

Thanks

 

3465.Timer0Script.pdf