This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365

1. Does the DM365 digital video output need to be buffered (for signal loading reasons)?

. YUV-4:2:0 would be better for processing the video for the USB interface.  RGB would be easier for the digital video output.  Can these both be generated simultaneously by the Front End?  (This may have been answered already as NO, but I'm not sure. It looked like the Resizer block had the option of having one output skip the Down sampler.  And the Video BE may be able to generate RGB from the IPIPE output?)

3.

Can the DM365 built-in DAC be used for the RGB output (rather than requiring a separate THS8200-type part)?  This may have been answered NO, because the DAC outputs seem to be limited to YPbPr.