Recently purchased a AM1808 eXperimenter Kit. I'm planning on using SYS/BIOS for a RTOS. Using CCS V4.1.3 but having problems building a BIOS project in CCS for this target. Is there a demo or quick start guide that guides a user through the steps necessary to build a SYS/BIOS example on this target. In trying to build the project I've selected a generic ARM9 target but without a configuration file I seem to have problems. Also do I need to use SYS/BIOS V6 or can I use SYS/BIOS v5?