This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: Loading PRU code firmware while booting

Part Number: AM6442
Other Parts Discussed in Thread: DP83869

Tool/software:

Hi All, 

I always getting following PRU cores firmware failed. Is there anything I need to enable or anything that makes these error go away. 


remoteproc remoteproc1: Direct firmware load for am64-main-r5f0_1-fw failed with error -2
[ 10.537447] remoteproc remoteproc3: Direct firmware load for am64-main-r5f1_1-fw failed with error -2
[ 10.547042] remoteproc remoteproc2: Direct firmware load for am64-main-r5f1_0-fw failed with error -2
[ 10.556649] remoteproc remoteproc0: Direct firmware load for am64-main-r5f0_0-fw failed with error -2
[ 10.564591] davinci_mdio 300b2400.mdio: phy[3]: device 300b2400.mdio:03, driver TI DP83869
[ 10.566153] remoteproc remoteproc2: powering up 78400000.r5f
[ 10.574614] davinci_mdio 300b2400.mdio: phy[15]: device 300b2400.mdio:0f, driver TI DP83869
[ 10.580365] remoteproc remoteproc3: powering up 78600000.r5f
[ 10.580473] remoteproc remoteproc3: Direct firmware load for am64-main-r5f1_1-fw failed with error -2
[ 10.590341] omap8250 2800000.serial: Configured USART0 for clock frequency 48MHz
[ 10.594790] remoteproc remoteproc0: powering up 78000000.r5f
[ 10.604806] printk: console [ttyS2] disabled
[ 10.611820] remoteproc remoteproc1: powering up 78200000.r5f
[ 10.611925] remoteproc remoteproc1: Direct firmware load for am64-main-r5f0_1-fw failed with error -2
[ 10.637242] remoteproc remoteproc2: Direct firmware load for am64-main-r5f1_0-fw failed with error -2
[ 10.637280] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 321, base_baud = 3000000) is a 8250
[ 10.646694] remoteproc remoteproc3: request_firmware failed: -2
[ 10.661577] printk: console [ttyS2] enabled
[ 10.661612] remoteproc remoteproc0: Direct firmware load for am64-main-r5f0_0-fw failed with error -2
[ 10.665781] printk: bootconsole [ns16550a0] disabled
[ 10.674994] remoteproc remoteproc2: request_firmware failed: -2
[ 10.661577] printk: console [ttyS2] enabled
[ 10.661612] remoteproc remoteproc0: Direct firmware load for am64-main-r5f0_0-fw failed with error -2
[ 10.665781] printk: bootconsole [ns16550a0] disabled
[ 10.674994] remoteproc remoteproc2: request_firmware failed: -2
[ 10.710678] remoteproc remoteproc1: request_firmware failed: -2

Using the follow .elf files

am65x-sr2-pru0-prueth-fw.elf
am65x-sr2-pru1-prueth-fw.elf
am65x-sr2-rtu0-prueth-fw.elf
am65x-sr2-rtu1-prueth-fw.elf
am65x-sr2-txpru0-prueth-fw.elf
am65x-sr2-txpru1-prueth-fw.elf