Other Parts Discussed in Thread: AM1808, AM1806
I'm building a CCS (v4.1.3) project that is using SYS/BIOS. The device is set to a generic ARM9 device and the RTSC Platform is ti.platforms.generic. When I try to build the project I get errors in the common.cfg file. The error list that the catalogName, deviceName and clockRate are not defined. How do I define these settings? I'm unable to edit the fields when I open up the common.cfg file in CCS and select properties. Also how are the catalogName and deviceName used and what types of information is in these two fields?