Part Number: SK-AM62P-LP
Tool/software:
Hello TI,
Can you help me to set the A53 clock frequency to maximum in sd card boot mode?
i verified that A53 was running at 1.2Ghz by default and maximum it can go 1.4Ghz so we want to set the frequency to 1.4Ghz.
root@am62pxx-evm:~# k3conf dump processor |------------------------------------------------------------------------------| | VERSION INFO | |------------------------------------------------------------------------------| | K3CONF | (version 0.3-nogit built Sat May 25 16:31:55 UTC 2024) | | SoC | AM62Px SR1.0 | | SYSFW | ABI: 3.1 (firmware version 0x0009 '9.2.8--v09.02.08 (Kool Koala))') | |------------------------------------------------------------------------------| |--------------------------------------------------------------------------------------| | Device ID | Processor ID | Processor Name | Processor State | Processor Frequency | |--------------------------------------------------------------------------------------| | 121 | 1 | WKUP_R5FSS0_CORE0 | DEVICE_STATE_ON | 800000000 | | 9 | 3 | MCU_R5FSS0_CORE0 | DEVICE_STATE_ON | 800000000 | | 135 | 32 | A53SS0_CORE_0 | DEVICE_STATE_ON | 1200000000 | | 136 | 33 | A53SS0_CORE_1 | DEVICE_STATE_ON | 1200000000 | | 137 | 34 | A53SS0_CORE_2 | DEVICE_STATE_ON | 1200000000 | | 138 | 35 | A53SS0_CORE_3 | DEVICE_STATE_ON | 1200000000 | | 225 | 128 | HSM0 | DEVICE_STATE_ON | 500000000 | |--------------------------------------------------------------------------------------|
i have followed soc initialization step in sbl boot and set 1.4Ghz and doesn't effecting in SD card boot mode,which requires a spl boot flow (as per my understanding). so can you please help me to do this?
Thank you.
Raj.