Tool/software:
Hi,
Using 9.2 SDK
I need to use the streaming engine functionality with addition to DMA. Just want to know which libs or headers files I need to include for it.
Need to use below code but getting undefined reference for all streaming engine related identifiers when compiling.
//Setup SE to fetch image array __STRM_TEMPLATE seTemplate; __STRM_PARAM_3D seParam; __SE_FLAGS seFlags; //Set flags to default seFlags = __SE_FLAGS_default() //Update necessary flags seFlags.ELETYPE = __SE_ELETYPE_8BIT; seFlags.VECLEN = __SE_VECLEN_64ELEMS; //Set params for 2D access seParam.ICNT0 = IMAGE_WIDTH; seParam.ICNT1 = IMAGE_HEIGHT; seParam.DIM1 = IMAGE_WIDTH; seParam.ICNT2 = 1; seParam.DIM2 = 0; //Create seTemplate seTemplate = __SE_SET_PARAM_3D(&seParam, &seFlags); //Open the stream __SE0_OPEN((void *)image, seTemplate);