This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
Once after the kernel and file system are up, I can see the mtd partitions under /proc/mtd/ .
But, mtd partitions are not listed when I run the df command or mount command.
Following mount command also fails.
#mount -t jffs2 /dev/mtdblock2 /mnt/testdir
Regards,
Prabhu
Once after the kernel and file system are up, I can see the mtd partitions under /proc/mtd/
Can you provide the output of `ls -al /dev/mtd*`?
Also, can you pls attach a complete Kernel log.
Following mount command also fails.
#mount -t jffs2 /dev/mtdblock2 /mnt/testdir
How does it fail (log)?
Regards, Andreas
Output for
mount -t jffs2 /dev/mtdblock2 /mnt/test
tried other types of file system.
That is also failed with the following output.
output for
#ls /dev/mtd*
output for
#mount
Output for
#df
mkfs commands available on the target.
Regards,
Prabhu
Dmesg log is also attached. Taken just after the kernel and file system are up.
dmesg [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 6.1.83-ti-gc1c2f1971fbf (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Mon May 13 20:19:51 UTC 2024 [ 0.000000] Machine model: Visteon AM62P5 Toyota Pre-sample A [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] OF: reserved mem: failed to allocate memory for node 'linux,cma': size 576 MiB [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c900000, size 30 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@9c900000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000bfffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009c7fffff] [ 0.000000] node 0: [mem 0x000000009c800000-0x000000009e6fffff] [ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff] [ 0.000000] node 0: [mem 0x000000009e780000-0x000000009fffffff] [ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000bfffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff] [ 0.000000] cma: Reserved 32 MiB at 0x00000000bcc00000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.5 [ 0.000000] percpu: Embedded 20 pages/cpu s41448 r8192 d32280 u81920 [ 0.000000] pcpu-alloc: s41448 r8192 d32280 u81920 alloc=20*4096 [ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] alternatives: applying boot alternatives [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 258048 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=/dev/mmcblk0p1 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 918336K/1048576K available (12096K kernel code, 1270K rwdata, 4076K rodata, 2048K init, 438K bss, 97472K reserved, 32768K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 256 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GICv3: GICv3 features: 16 PPIs [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @82400000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000081840000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000081850000 [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention. [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.000261] Console: colour dummy device 80x25 [ 0.000304] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.000315] pid_max: default: 32768 minimum: 301 [ 0.000361] LSM: Security Framework initializing [ 0.000461] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear) [ 0.000473] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear) [ 0.001885] cblist_init_generic: Setting adjustable number of callback queues. [ 0.001900] cblist_init_generic: Setting shift to 2 and lim to 1. [ 0.001961] cblist_init_generic: Setting adjustable number of callback queues. [ 0.001966] cblist_init_generic: Setting shift to 2 and lim to 1. [ 0.002104] rcu: Hierarchical SRCU implementation. [ 0.002109] rcu: Max phase no-delay instances is 1000. [ 0.002325] Platform MSI: msi-controller@1820000 domain created [ 0.002469] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.002644] EFI services will not be available. [ 0.002850] smp: Bringing up secondary CPUs ... [ 0.003402] Detected VIPT I-cache on CPU1 [ 0.003489] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 0.003504] GICv3: CPU1: using allocated LPI pending table @0x0000000081860000 [ 0.003551] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.004197] Detected VIPT I-cache on CPU2 [ 0.004269] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000 [ 0.004283] GICv3: CPU2: using allocated LPI pending table @0x0000000081870000 [ 0.004313] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 0.004853] Detected VIPT I-cache on CPU3 [ 0.004923] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000 [ 0.004934] GICv3: CPU3: using allocated LPI pending table @0x0000000081880000 [ 0.004961] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 0.005024] smp: Brought up 1 node, 4 CPUs [ 0.005038] SMP: Total of 4 processors activated. [ 0.005043] CPU features: detected: 32-bit EL0 Support [ 0.005048] CPU features: detected: CRC32 instructions [ 0.005100] CPU: All CPU(s) started at EL2 [ 0.005104] alternatives: applying system-wide alternatives [ 0.006307] devtmpfs: initialized [ 0.012659] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.012688] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [ 0.013767] pinctrl core: initialized pinctrl subsystem [ 0.014272] DMI not present or invalid. [ 0.014809] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.015815] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations [ 0.016037] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.016129] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.016196] audit: initializing netlink subsys (disabled) [ 0.016336] audit: type=2000 audit(0.016:1): state=initialized audit_enabled=0 res=1 [ 0.016725] thermal_sys: Registered thermal governor 'step_wise' [ 0.016731] thermal_sys: Registered thermal governor 'power_allocator' [ 0.016769] cpuidle: using governor menu [ 0.016899] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.016980] ASID allocator initialised with 65536 entries [ 0.026621] platform 30200000.dss: Fixed dependency cycle(s) with /display [ 0.026679] platform display: Fixed dependency cycle(s) with /bus@f0000/dss@30200000 [ 0.027046] KASLR disabled due to lack of seed [ 0.033292] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages [ 0.033305] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page [ 0.033311] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages [ 0.033315] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page [ 0.033320] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages [ 0.033323] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page [ 0.033328] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages [ 0.033332] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page [ 0.034515] k3-chipinfo 43000014.chipid: Family:AM62PX rev:SR1.0 JTAGID[0x0bb9d02f] Detected [ 0.034993] iommu: Default domain type: Translated [ 0.034999] iommu: DMA domain TLB invalidation policy: strict mode [ 0.035019] Einstein_gpios_pins_init [ 0.035303] SCSI subsystem initialized [ 0.035419] libata version 3.00 loaded. [ 0.035589] usbcore: registered new interface driver usbfs [ 0.035620] usbcore: registered new interface driver hub [ 0.035643] usbcore: registered new device driver usb [ 0.035928] pps_core: LinuxPPS API ver. 1 registered [ 0.035933] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.035945] PTP clock support registered [ 0.036050] EDAC MC: Ver: 3.0.0 [ 0.036774] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fca100 [ 0.036844] omap-mailbox 29010000.mailbox: no available mbox devices found [ 0.036879] omap-mailbox 29020000.mailbox: no available mbox devices found [ 0.036912] omap-mailbox 29030000.mailbox: no available mbox devices found [ 0.037212] FPGA manager framework [ 0.037285] Advanced Linux Sound Architecture Driver Initialized. [ 0.038065] clocksource: Switched to clocksource arch_sys_counter [ 0.038262] VFS: Disk quotas dquot_6.6.0 [ 0.038297] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.043635] NET: Registered PF_INET protocol family [ 0.043916] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.044977] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear) [ 0.045000] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.045012] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.045072] TCP bind hash table entries: 8192 (order: 6, 262144 bytes, linear) [ 0.045274] TCP: Hash tables configured (established 8192 bind 8192) [ 0.045381] UDP hash table entries: 512 (order: 2, 16384 bytes, linear) [ 0.045414] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear) [ 0.045558] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.045973] RPC: Registered named UNIX socket transport module. [ 0.045982] RPC: Registered udp transport module. [ 0.045986] RPC: Registered tcp transport module. [ 0.045989] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.045997] NET: Registered PF_XDP protocol family [ 0.046011] PCI: CLS 0 bytes, default 64 [ 0.046700] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.048030] Initialise system trusted keyrings [ 0.048235] workingset: timestamp_bits=46 max_order=18 bucket_order=0 [ 0.052259] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.052785] NFS: Registering the id_resolver key type [ 0.052814] Key type id_resolver registered [ 0.052818] Key type id_legacy registered [ 0.052871] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.052877] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.088025] Key type asymmetric registered [ 0.088035] Asymmetric key parser 'x509' registered [ 0.088080] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.088219] io scheduler mq-deadline registered [ 0.088226] io scheduler kyber registered [ 0.091000] pinctrl-single 4084000.pinctrl: 34 pins, size 136 [ 0.091541] pinctrl-single f4000.pinctrl: 171 pins, size 684 [ 0.097014] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled [ 0.101711] panel-simple display: supply power not found, using dummy regulator [ 0.101876] ------------[ cut here ]------------ [ 0.101882] WARNING: CPU: 0 PID: 1 at drivers/gpu/drm/panel/panel-simple.c:616 panel_simple_probe+0x2fc/0x3b0 [ 0.101903] Modules linked in: [ 0.101913] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 6.1.83-ti-gc1c2f1971fbf #1 [ 0.101921] Hardware name: Visteon AM62P5 Toyota Pre-sample A (DT) [ 0.101926] pstate: 00000005 (nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 0.101934] pc : panel_simple_probe+0x2fc/0x3b0 [ 0.101944] lr : panel_simple_probe+0xdc/0x3b0 [ 0.101953] sp : ffff8000093ebaf0 [ 0.101956] x29: ffff8000093ebb70 x28: 0000000000000000 x27: ffff800008ff00c8 [ 0.101969] x26: ffff800009076060 x25: ffff800009076078 x24: 0000000000000000 [ 0.101980] x23: ffff800009382a38 x22: ffff800008c9e510 x21: ffff0000028b9410 [ 0.101992] x20: ffff000001aae280 x19: 0000000000000007 x18: ffffffffffffffff [ 0.102004] x17: 616c756765722079 x16: 6d6d756420676e69 x15: ffff00000182ea1c [ 0.102015] x14: 0000000000000000 x13: 00302e726f74616c x12: 756765723a726f74 [ 0.102027] x11: 2d2d302e726f7461 x10: 0000000000060280 x9 : 0000000000000004 [ 0.102038] x8 : 0101010101010101 x7 : 7f7f7f7f7f7f7f7f x6 : fefefeff666d686c [ 0.102050] x5 : 8080808000000000 x4 : 0000000000000000 x3 : ffff800009390f50 [ 0.102061] x2 : 0000000000000000 x1 : 0000000000000046 x0 : 00000000ffffffcc [ 0.102074] Call trace: [ 0.102078] panel_simple_probe+0x2fc/0x3b0 [ 0.102088] panel_simple_platform_probe+0x34/0x4c [ 0.102098] platform_probe+0x68/0xe0 [ 0.102108] really_probe+0xbc/0x2dc [ 0.102115] __driver_probe_device+0x78/0x114 [ 0.102122] driver_probe_device+0xd8/0x15c [ 0.102129] __driver_attach+0x94/0x19c [ 0.102136] bus_for_each_dev+0x74/0xd4 [ 0.102142] driver_attach+0x24/0x30 [ 0.102149] bus_add_driver+0x154/0x20c [ 0.102155] driver_register+0x78/0x130 [ 0.102162] __platform_driver_register+0x28/0x34 [ 0.102170] panel_simple_init+0x24/0x64 [ 0.102181] do_one_initcall+0x54/0x1d0 [ 0.102189] kernel_init_freeable+0x218/0x284 [ 0.102199] kernel_init+0x24/0x130 [ 0.102209] ret_from_fork+0x10/0x20 [ 0.102217] ---[ end trace 0000000000000000 ]--- [ 0.102269] ------------[ cut here ]------------ [ 0.102273] WARNING: CPU: 0 PID: 1 at drivers/gpu/drm/panel/panel-simple.c:621 panel_simple_probe+0x30c/0x3b0 [ 0.102287] Modules linked in: [ 0.102292] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 6.1.83-ti-gc1c2f1971fbf #1 [ 0.102299] Hardware name: Visteon AM62P5 Toyota Pre-sample A (DT) [ 0.102302] pstate: a0000005 (NzCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 0.102309] pc : panel_simple_probe+0x30c/0x3b0 [ 0.102318] lr : panel_simple_probe+0xdc/0x3b0 [ 0.102327] sp : ffff8000093ebaf0 [ 0.102331] x29: ffff8000093ebb70 x28: 0000000000000000 x27: ffff800008ff00c8 [ 0.102343] x26: ffff800009076060 x25: ffff800009076078 x24: 0000000000000000 [ 0.102354] x23: ffff800009382a38 x22: ffff800008c9e510 x21: ffff0000028b9410 [ 0.102366] x20: ffff000001aae280 x19: 0000000000000007 x18: ffffffffffffffff [ 0.102377] x17: 616c756765722079 x16: 6d6d756420676e69 x15: ffff00000182ea1c [ 0.102389] x14: 0000000000000000 x13: 00302e726f74616c x12: 756765723a726f74 [ 0.102400] x11: 2d2d302e726f7461 x10: 0000000000060280 x9 : 0000000000000004 [ 0.102412] x8 : 0101010101010101 x7 : 7f7f7f7f7f7f7f7f x6 : fefefeff666d686c [ 0.102423] x5 : 8080808000000000 x4 : 0000000000000000 x3 : ffff800009390f50 [ 0.102434] x2 : 00000000ffffeff0 x1 : 00000000fffffffa x0 : 000000000000100a [ 0.102446] Call trace: [ 0.102448] panel_simple_probe+0x30c/0x3b0 [ 0.102458] panel_simple_platform_probe+0x34/0x4c [ 0.102468] platform_probe+0x68/0xe0 [ 0.102476] really_probe+0xbc/0x2dc [ 0.102482] __driver_probe_device+0x78/0x114 [ 0.102489] driver_probe_device+0xd8/0x15c [ 0.102496] __driver_attach+0x94/0x19c [ 0.102503] bus_for_each_dev+0x74/0xd4 [ 0.102509] driver_attach+0x24/0x30 [ 0.102515] bus_add_driver+0x154/0x20c [ 0.102521] driver_register+0x78/0x130 [ 0.102528] __platform_driver_register+0x28/0x34 [ 0.102536] panel_simple_init+0x24/0x64 [ 0.102544] do_one_initcall+0x54/0x1d0 [ 0.102551] kernel_init_freeable+0x218/0x284 [ 0.102559] kernel_init+0x24/0x130 [ 0.102566] ret_from_fork+0x10/0x20 [ 0.102573] ---[ end trace 0000000000000000 ]--- [ 0.107899] loop: module loaded [ 0.108781] megasas: 07.719.03.00-rc1 [ 0.111511] tun: Universal TUN/TAP device driver, 1.6 [ 0.112095] VFIO - User Level meta-driver version: 0.3 [ 0.112710] usbcore: registered new interface driver usb-storage [ 0.113162] i2c_dev: i2c /dev entries driver [ 0.114401] sdhci: Secure Digital Host Controller Interface driver [ 0.114412] sdhci: Copyright(c) Pierre Ossman [ 0.114573] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.115079] ledtrig-cpu: registered to indicate activity on CPUs [ 0.115219] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.115512] usbcore: registered new interface driver usbhid [ 0.115517] usbhid: USB HID core driver [ 0.116245] optee: probing for conduit method. [ 0.116274] optee: revision 4.1 (012cdca4) [ 0.116517] optee: dynamic shared memory is enabled [ 0.116736] optee: initialized driver [ 0.117906] Initializing XFRM netlink socket [ 0.117937] NET: Registered PF_PACKET protocol family [ 0.118006] Key type dns_resolver registered [ 0.118382] registered taskstats version 1 [ 0.118405] Loading compiled-in X.509 certificates [ 0.126181] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.2.7--v09.02.07 (Kool Koala)') [ 0.159910] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created [ 0.160043] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created [ 0.160241] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created [ 0.160479] ti-sci-inta 4e400000.interrupt-controller: Interrupt Aggregator domain 200 created [ 0.161047] ti-udma 485c0100.dma-controller: Number of rings: 82 [ 0.162859] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18) [ 0.165015] ti-udma 485c0000.dma-controller: Number of rings: 150 [ 0.168382] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15) [ 0.170096] ti-udma 4e230000.dma-controller: Number of rings: 6 [ 0.170489] ti-udma 4e230000.dma-controller: Channels: 6 (bchan: 0, tchan: 0, rchan: 6) [ 0.171473] printk: console [ttyS2] disabled [ 0.171534] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 248, base_baud = 3000000) is a 8250 [ 0.171600] printk: console [ttyS2] enabled [ 0.171605] printk: bootconsole [ns16550a0] disabled [ 0.172482] 2840000.serial: ttyS4 at MMIO 0x2840000 (irq = 249, base_baud = 3000000) is a 8250 [ 0.175614] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0 [ 0.179374] Console: switching to colour frame buffer device 240x45 [ 0.205789] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device [ 0.207924] spi-nor spi0.0: mx25uw12845g (16384 Kbytes) [ 0.208012] 3 fixed-partitions partitions found on MTD device fc40000.spi.0 [ 0.208021] Creating 3 MTD partitions on "fc40000.spi.0": [ 0.208027] 0x000000000000-0x000000080000 : "SBL_STAGE1" [ 0.209140] 0x000000080000-0x000000100000 : "SBL_STAGE2" [ 0.210097] 0x000000100000-0x000000200000 : "DM_APP" [ 0.213896] mmc0: CQHCI version 5.10 [ 0.255158] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit [ 0.328761] mmc0: Command Queue Engine enabled [ 0.328830] mmc0: new HS400 MMC card at address 0001 [ 0.331080] mmcblk0: mmc0:0001 8GUF4R 7.28 GiB [ 0.337375] mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 p16 [ 0.339493] mmcblk0boot0: mmc0:0001 8GUF4R 31.9 MiB [ 0.340438] mmcblk0boot1: mmc0:0001 8GUF4R 31.9 MiB [ 0.341252] mmcblk0rpmb: mmc0:0001 8GUF4R 4.00 MiB, chardev (240:0) [ 1.122968] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present! [ 1.123274] debugfs: Directory 'pd:244' with parent 'pm_genpd' already present! [ 1.130051] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present! [ 1.130165] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present! [ 1.139230] ALSA device list: [ 1.139248] No soundcards found. [ 1.143756] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Quota mode: none. [ 1.144283] VFS: Mounted root (ext4 filesystem) on device 179:1. [ 1.146154] devtmpfs: mounted [ 1.146823] Freeing unused kernel memory: 2048K [ 1.146930] Run /sbin/init as init process [ 1.146937] with arguments: [ 1.146940] /sbin/init [ 1.146942] with environment: [ 1.146945] HOME=/ [ 1.146948] TERM=linux [ 1.225408] pvrsrvkm: loading out-of-tree module taints kernel. [ 1.240197] PVR_K: 135: Device: fd80000.gpu [ 1.241078] PVR_K: 135: Read BVNC 36.53.104.796 from HW device registers [ 1.241122] PVR_K: 135: RGX Device registered BVNC 36.53.104.796 with 1 core in the system [ 1.241718] [drm] Initialized pvr 23.3.6512818 20170530 for fd80000.gpu on minor 1 [ 1.293741] systemd[1]: System time before build time, advancing clock. [ 1.320200] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid) [ 1.321024] systemd[1]: Detected architecture arm64. [ 1.375206] systemd[1]: Hostname set to <am62pxx-einstein>. [ 1.914695] systemd[1]: Configuration file /etc/systemd/system/vmf.service is marked executable. Please remove executable permission bits. Proceeding anyway. [ 1.944564] systemd[1]: Configuration file /etc/systemd/system/dlt-daemon.service is marked executable. Please remove executable permission bits. Proceeding anyway. [ 1.945625] systemd[1]: Configuration file /etc/systemd/system/display-static-image.service is marked executable. Please remove executable permission bits. Proceeding anyway. [ 2.014150] systemd[1]: Queued start job for default target Multi-User System. [ 2.061633] systemd[1]: Created slice Slice /system/getty. [ 2.063631] systemd[1]: Created slice Slice /system/modprobe. [ 2.065303] systemd[1]: Created slice Slice /system/serial-getty. [ 2.066793] systemd[1]: Created slice User and Session Slice. [ 2.067164] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ 2.067419] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ 2.067744] systemd[1]: Reached target Path Units. [ 2.067850] systemd[1]: Reached target Remote File Systems. [ 2.067928] systemd[1]: Reached target Slice Units. [ 2.068037] systemd[1]: Reached target Swaps. [ 2.068656] systemd[1]: Listening on Syslog Socket. [ 2.068991] systemd[1]: Listening on initctl Compatibility Named Pipe. [ 2.069653] systemd[1]: Listening on Journal Audit Socket. [ 2.070029] systemd[1]: Listening on Journal Socket (/dev/log). [ 2.070548] systemd[1]: Listening on Journal Socket. [ 2.071156] systemd[1]: Listening on Network Service Netlink Socket. [ 2.071740] systemd[1]: Listening on udev Control Socket. [ 2.072097] systemd[1]: Listening on udev Kernel Socket. [ 2.072460] systemd[1]: Listening on User Database Manager Socket. [ 2.076146] systemd[1]: Mounting Huge Pages File System... [ 2.080274] systemd[1]: Mounting POSIX Message Queue File System... [ 2.084802] systemd[1]: Mounting Kernel Debug File System... [ 2.085445] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing). [ 2.090238] systemd[1]: Mounting Temporary Directory /tmp... [ 2.095261] systemd[1]: Starting Create List of Static Device Nodes... [ 2.100086] systemd[1]: Starting Load Kernel Module configfs... [ 2.104683] systemd[1]: Starting Load Kernel Module drm... [ 2.108589] configfs: exports duplicate symbol config_group_find_item (owned by kernel) [ 2.109791] systemd[1]: Starting Load Kernel Module fuse... [ 2.110200] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/). [ 2.116602] systemd[1]: Starting Journal Service... [ 2.118381] systemd[1]: Load Kernel Modules was skipped because all trigger condition checks failed. [ 2.119933] fuse: init (API version 7.37) [ 2.123329] systemd[1]: Starting Generate network units from Kernel command line... [ 2.128045] systemd[1]: Starting Remount Root and Kernel File Systems... [ 2.133102] systemd[1]: Starting Apply Kernel Variables... [ 2.138165] systemd[1]: Starting Coldplug All udev Devices... [ 2.146666] systemd[1]: Mounted Huge Pages File System. [ 2.147445] systemd[1]: Mounted POSIX Message Queue File System. [ 2.148234] systemd[1]: Mounted Kernel Debug File System. [ 2.149116] systemd[1]: Mounted Temporary Directory /tmp. [ 2.163853] EXT4-fs (mmcblk0p1): re-mounted. Quota mode: none. [ 2.167282] systemd[1]: Finished Create List of Static Device Nodes. [ 2.174593] systemd[1]: modprobe@drm.service: Deactivated successfully. [ 2.175578] systemd[1]: Finished Load Kernel Module drm. [ 2.179085] systemd[1]: modprobe@fuse.service: Deactivated successfully. [ 2.180066] systemd[1]: Finished Load Kernel Module fuse. [ 2.181728] systemd[1]: Finished Generate network units from Kernel command line. [ 2.183555] systemd[1]: modprobe@configfs.service: Deactivated successfully. [ 2.184473] systemd[1]: Finished Load Kernel Module configfs. [ 2.186000] systemd[1]: Finished Remount Root and Kernel File Systems. [ 2.186894] systemd[1]: Reached target Preparation for Network. [ 2.191240] systemd[1]: Mounting FUSE Control File System... [ 2.195828] systemd[1]: Mounting Kernel Configuration File System... [ 2.197518] systemd[1]: Rebuild Hardware Database was skipped because of a failed condition check (ConditionNeedsUpdate=/etc). [ 2.197910] systemd[1]: Platform Persistent Storage Archival was skipped because of a failed condition check (ConditionDirectoryNotEmpty=/sys/fs/pstore). [ 2.198324] systemd[1]: Create System Users was skipped because of a failed condition check (ConditionNeedsUpdate=/etc). [ 2.203920] systemd[1]: Starting Create Static Device Nodes in /dev... [ 2.207762] systemd[1]: Mounted FUSE Control File System. [ 2.216090] systemd[1]: Finished Apply Kernel Variables. [ 2.220727] systemd[1]: Mounted Kernel Configuration File System. [ 2.240201] systemd[1]: Finished Create Static Device Nodes in /dev. [ 2.240689] systemd[1]: Reached target Preparation for Local File Systems. [ 2.244360] audit: type=1334 audit(1651167745.948:2): prog-id=5 op=LOAD [ 2.244687] audit: type=1334 audit(1651167745.948:3): prog-id=6 op=LOAD [ 2.264928] systemd[1]: Starting Rule-based Manager for Device Events and Files... [ 2.265533] systemd[1]: Started Journal Service. [ 2.297664] systemd-journald[163]: Received client request to flush runtime journal. [ 2.610110] random: crng init done [ 2.676423] PVR_K: 143: RGX Firmware image 'rgx.fw.36.53.104.796' loaded [ 2.692560] PVR_K: 143: Shader binary image 'rgx.sh.36.53.104.796' loaded [ 2.846318] rtc-ti-k3 2b1f0000.rtc: Clock rate 32552 is not 32768! Could misbehave! [ 2.862725] rtc-ti-k3 2b1f0000.rtc: registered as rtc0 [ 2.863212] rtc-ti-k3 2b1f0000.rtc: setting system clock to 1970-01-01T00:00:03 UTC (3) [ 2.866897] systemd-journald[163]: Time jumped backwards, rotating. [ 2.900251] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1) [ 2.913631] platform 78000000.r5f: configured R5F for IPC-only mode [ 2.913776] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9c800000 [ 2.914555] remoteproc remoteproc0: 78000000.r5f is available [ 2.914638] remoteproc remoteproc0: attaching to 78000000.r5f [ 2.914731] platform 78000000.r5f: R5F core initialized in IPC-only mode [ 2.914738] remoteproc remoteproc0: remote processor 78000000.r5f is now attached [ 3.291286] dwc3 31100000.usb: Configuration mismatch. dr_mode forced to gadget [ 3.335623] usbcore: exports duplicate symbol cdc_parse_cdc_header (owned by kernel) [ 3.395850] EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Quota mode: none. [ 3.401093] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Quota mode: none. [ 3.417486] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Quota mode: none. [ 3.800966] systemd-journald[163]: Oldest entry in /run/log/journal/63effb0abed54a408d903ac0f06915be/system.journal is older than the configured file retention duration (1month), suggesting rotation. [ 3.800999] systemd-journald[163]: /run/log/journal/63effb0abed54a408d903ac0f06915be/system.journal: Journal header limits reached or header out-of-date, rotating. [ 3.888709] audit: type=1334 audit(1651168941.900:4): prog-id=7 op=LOAD [ 3.889125] audit: type=1334 audit(1651168941.900:5): prog-id=8 op=LOAD [ 8.458172] audit: type=1334 audit(1651168946.468:6): prog-id=9 op=LOAD [ 8.459089] audit: type=1334 audit(1651168946.472:7): prog-id=10 op=LOAD [ 8.825001] audit: type=1006 audit(1651168946.836:8): pid=272 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1 [ 8.825035] audit: type=1300 audit(1651168946.836:8): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffde502a40 a2=1 a3=ffff9d0f6020 items=0 ppid=1 pid=272 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null) [ 8.825047] audit: type=1327 audit(1651168946.836:8): proctitle="(systemd)" [ 8.852917] audit: type=1334 audit(1651168946.864:9): prog-id=11 op=LOAD [ 8.852948] audit: type=1300 audit(1651168946.864:9): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffe5ce6f60 a2=78 a3=0 items=0 ppid=1 pid=272 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="systemd" exe="/lib/systemd/systemd" key=(null) [ 8.852960] audit: type=1327 audit(1651168946.864:9): proctitle="(systemd)" [ 8.852973] audit: type=1334 audit(1651168946.864:10): prog-id=11 op=UNLOAD [ 8.853088] audit: type=1334 audit(1651168946.864:11): prog-id=12 op=LOAD root@am62pxx-einstein@18:03:31:~# root@am62pxx-einstein@18:03:36:~# root@am62pxx-einstein@18:03:36:~#
Regards,
Prabhu
Thanks for the additional info, will review first thing next week.
Regards, Andreas
Hi Prabhu,
so reviewing what you sent I see evidence in several places that the Kernel is aware of the following (and only those) flash regions/partitions:
[ 0.208027] 0x000000000000-0x000000080000 : "SBL_STAGE1"
[ 0.209140] 0x000000080000-0x000000100000 : "SBL_STAGE2"
[ 0.210097] 0x000000100000-0x000000200000 : "DM_APP"
...which get exposed to the system through /dev/mtd*{0,1,2}
All these are raw partitions, containing straight binary firmware images. There is no filesystem associated with those partitions, hence mounting those won't work.
If you want to access these raw-data containing partitions you should use the character device for this. For example, to see the contents of the partition that holds "SBL_STAGE1" you would do this (on my system it's all 0xff - erased)
root@am62pxx-evm:~# hexdump -C /dev/mtd0 | head 00000000 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff |................| * 00080000
I suppose you are using an SBL-based bootflow, using the bootloader from the MCU+ SDK. If you want to have a filesystem on your flash you need to edit the device tree file to define additional partition(s), which you can then format with a specific filesystem (using `mkfs.xxxx`), and then you can mount them.
Regards, Andreas