This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: McASP GBLCTL write error

Part Number: AM625

Tool/software:

Hi expert,

Our customer is using SDK9.0 in the custom board. Below is the HW connection. AM62X is slave and AK2401A is Master which can work properly.

They config McASP as I2S, 2 channel, 32bit. AK2401A provide the FS/CLK, 72k/4.608MHz. But they found the McASP GBLCTL get below error and cannot sync up properly

Below is the register readout. Could you please help to check the possible reason? Thanks

0x2b10000 0x44307b02
0x2b10004 0x2 
0x2b10010 0x0 
0x2b10014 0x0  
0x2b10018 0x0 

B 1011
3 0011
9 1011
1 0001
0x2b1001c 

0x2b10044  0x2  - only RHCLKRST is set to 1   GBLCTL


0x2b10048 0x0 
0x2b1004C 0x0
0x2b10050 0x0
0x2b10060 0x1f  -RGBLCTL is 1f,but GBLCTL is 0x2?
0x2b10064 0xffffffff
0x2b10068 0x180f0 
0x2b1006c 0x111
0x2b10070 0x180080
0x2b10074 0x0
0x2b10078 0x3 
0x2b1007c 0x1  
0x2b10080 0x0 
0x2b10084 0x0
0x2b10088 0xff0008
0x2b1008c 0x0

Best Regards,

Xingyu Zhu