Part Number: SK-AM62B-P1
Tool/software:
Hi,
I have done a YOCTO build for am62xx , and I have enabled USB, DFU properties using u-boot menuconfig,
When I try to boot using tiboot3, it shows the following error:
U-Boot SPL 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)')
SPL initial stack usage: 13408 bytes
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
i also checks with SDK , it works fine for me .
can you provide me which all configs as to be enabled (r5,a53) for the correct yocto build ..
Regards,
-RJ