I have a 816x/389x evm development board with psp04.00.00.12 running on it. The usb port 1 does not seem to work in usb device mode. Will usb port 1 work in either host or device mode? It works fine on usb port 0.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a 816x/389x evm development board with psp04.00.00.12 running on it. The usb port 1 does not seem to work in usb device mode. Will usb port 1 work in either host or device mode? It works fine on usb port 0.
Thanks.
Hi,
Are you using Linux or are you developing custom applications?
Best regards, Zegeye
Steve,
I have some additional info for you:
The PSP release 4.00.01.13 has support to configure USB0/USB1 port to either device mode or host mode through menuconfig, refer to user's guide for more info.
The PSP release 4.00.00.12 supports only usb0 in device mode.
Regards,
Marc