Hello,
until now i have used the TMS320f28335 uC in my solutions. Now I need more computation power. So I have bought the TMDXEVM6472 hoping to use six cores to perform computations.
Unfortunatly I'm not able to connect the Vinculum 1 (ftdi) chip to my development board using sci, usart or spi because there are no such interfaces in TMS320C6472. Is it possible to use those RapidIO serials or other periferals to emulate usart communication? I need to transfer about 1.5 Mbit of data so the onboard i2c with max3221 is to slow for this communication.
topology:
[usb:slave device] <---usb---> [usb:host vncl1 ftdi] <---spi/uart with handshaking---> [evm6472]
Thanks for help
Maciek Łaski