Part Number: AM62A3-Q1
Tool/software:
Hello,I have some doubts about PDN simulation (Power SI), please help to solve it
1、Do I need to separate VDD_CORE-1 to 17 for simulation, or use VDD_CORE as a Port?
2、Do I need to include the PMIC FB loop in the simulation?
3、 Is the simulation starting frequency from 1Hz or from a minimum of 100kHz for the capacitor S2P?