Tool/software:
Hi,
The U-Boot provided with the Processor SDK 10.00.07.04 is configured to launch Linux from SD card (MMC1) and doesn't have saveenv enabled so I've modified board-support/ti-boot/board/ti/am64x/am64x.env to launch from MMC0 as follows
-mmcdev=1-bootpart=1:2+mmcdev=0+bootpart=0:1u-boot-am64xx-evm.img and tispl.bin-am64xx-evm have both been updated and reflashed both to the boot0 partition. I'm guess I didn't need to reflash tispl.bin but did that just to be on the safe side.
þ U-Boot SPL 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) Resetting on cold boot to workaround ErrataID:i2331 Please resend tiboot3.bin in case of UART/DFU boot resetting ... U-Boot SPL 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 13392 bytes Trying to boot from MMC1 Authentication passed Authentication passed Loading Environment from MMC... *** Warning - bad CRC, using default environment init_env from device 9 not supported! Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 I/TC: I/TC: OP-TEE version: 4.2.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Apr 12 09:51:21 UTC 2024 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: GIC redistributor base address not provided I/TC: Assuming default GIC group status and modifier I/TC: SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') Trying to boot from MMC1 Authentication passed Authentication passed U-Boot 2024.04-ti-gfda88f8bcea3 (Jul 26 2024 - 11:00:12 +0000) SoC: AM64X SR2.0 HS-FS Model: Texas Instruments AM642 EVM Board: AM64-EVM rev C DRAM: 2 GiB Core: 98 devices, 31 uclasses, devicetree: separate NAND: 0 MiB MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: eth0: ethernet@8000000port@1, eth2: icssg1-eth-port@0 Hit any key to stop autoboot: 0 MMC: no card present MMC: no card present ** Bad device specification mmc 1 ** MMC: no card present ** Bad device specification mmc 1 ** Couldn't find partition mmc 1:2 Can't set block device MMC: no card present ** Bad device specification mmc 1 ** Couldn't find partition mmc 1:2 Can't set block device libfdt fdt_check_header(): FDT_ERR_BADMAGIC No FDT memory address configured. Please configure the FDT address via "fdt addr <address>" command. Aborting! Bad Linux ARM64 Image magic! Scanning for bootflows in all bootdevs Seq Method State Uclass Part Name Filename --- ----------- ------ -------- ---- ------------------------ ---------------- Scanning global bootmeth 'efi_mgr': MMC: no card present No EFI system partition No EFI system partition Failed to persist EFI variables No EFI system partition Failed to persist EFI variables No EFI system partition Failed to persist EFI variables 0 efi_mgr ready (none) 0 <NULL> ** Booting bootflow '<NULL>' with efi_mgr Loading Boot0000 'mmc 0' failed EFI boot manager: Cannot load any image Boot failed (err=-14) Scanning bootdev 'mmc@fa00000.bootdev': MMC: no card present MMC: no card present MMC: no card present MMC: no card present Scanning bootdev 'mmc@fa10000.bootdev': No working controllers found link up on port 1, speed 1000, full duplex BOOTP broadcast 1 DHCP client bound to address 192.168.10.6 (114 ms) Scanning bootdev 'port@1.bootdev': missing environment variable: pxeuuid Retrieving file: pxelinux.cfg/01-34-08-e1-80-b7-b3 link up on port 1, speed 1000, full duplex Using ethernet@8000000port@1 device TFTP from server 192.168.10.1; our IP address is 192.168.10.6 Filename 'pxelinux.cfg/01-34-08-e1-80-b7-b3'. Load address: 0x80100000 Loading: *
U-Boot # setenv mmcdev 0 U-Boot # setenv bootpart 0 U-Boot # boot