Part Number: AM625
Other Parts Discussed in Thread: SK-AM62
Tool/software:
Hi, Experts:
we used tiboot3-am62x-gp-evm.bin, tispl.bin_unsigned,u-boot.img_unsigned,
and the SD card startup has failed as follows(on both custom or SK_EVM_E3):
U-Boot SPL 2024.04 (Oct 12 2024 - 14:45:39 +0800)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
SPL initial stack usage: 13392 bytes
Trying to boot from MMC2
Starting ATF on ARM64 core...
NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty
NOTICE: BL31: Built : 16:09:05, Feb 9 2024
ERROR: Timeout waiting for thread SP_RESPONSE to fill
ERROR: Thread SP_RESPONSE verification failed (-60)
ERROR: Message receive failed (-60)
ERROR: Failed to get response (-60)
ERROR: Transfer send failed (-60)
ERROR: Timeout waiting for thread SP_RESPONSE to fill
ERROR: Thread SP_RESPONSE verification failed (-60)
ERROR: Message receive failed (-60)
ERROR: Failed to get response (-60)
ERROR: Transfer send failed (-60)
ERROR: Unable to query firmware capabilities (-60)
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 ti_sci_init:486 Unable to communicate with control firmware (-65523)
E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x00070568 failed
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 tee_otp_get_hw_unique_key:97 Could not get HUK
E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x00070590 failed
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 sa2ul_init:106 Could not change TRNG firewall owner
E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x00070598 failed
E/TC:0 0
E/TC:0 0 Core data-abort at address 0x14 (translation fault)
E/TC:0 0 esr 0x96000005 ttbr0 0x9e8a1000 ttbr1 0x00000000 cidr 0x0
E/TC:0 0 cpu #0 cpsr 0x600003c4
E/TC:0 0 x0 000000009e874000 x1 0000000000000000
E/TC:0 0 x2 0000000000000000 x3 0000000000000000
E/TC:0 0 x4 0000000000000050 x5 000000009e891d70
E/TC:0 0 x6 ffffffffffffffb0 x7 0000000000010cb0
E/TC:0 0 x8 0000000000010cb0 x9 000000009e891f80
E/TC:0 0 x10 000000009e881070 x11 0000000000000008
E/TC:0 0 x12 0000000000000000 x13 000000009e8a2e60
E/TC:0 0 x14 0000000000000000 x15 0000000000000000
E/TC:0 0 x16 000000009e81c74c x17 0000000000000000
E/TC:0 0 x18 0000000000000000 x19 000000009e8a31e0
E/TC:0 0 x20 000000009e8a31e8 x21 000000009e874000
E/TC:0 0 x22 000000009e874000 x23 000000009e874f00
E/TC:0 0 x24 000000009e873dc0 x25 0000000000000000
E/TC:0 0 x26 0000000000000000 x27 0000000000000000
E/TC:0 0 x28 0000000000000000 x29 000000009e8a3170
E/TC:0 0 x30 000000009e816f6c elr 000000009e816f7c
E/TC:0 0 sp_el0 000000009e8a3170
E/TC:0 0 TEE load address @ 0x9e800000
E/TC:0 0 Call stack:
E/TC:0 0 0x9e816f7c
E/TC:0 0 0x9e807c64
E/TC:0 0 0x9e8220ec
E/TC:0 0 0x9e807de0
E/TC:0 0 Panic 'unhandled pageable abort' at /usr/src/debug/optee-os/4.2.0+git/core/arch/arm/kernel/abort.c:582 <abort_handler>
E/TC:0 0 TEE load address @ 0x9e800000
E/TC:0 0 Call stack:
E/TC:0 0 0x9e808030
E/TC:0 0 0x9e81ebb0
E/TC:0 0 0x9e807884
E/TC:0 0 0x9e804a68
so, how to used the SDK10 on GP device?