Other Parts Discussed in Thread: SYSBIOS
Hello BIOS experts,
Here is my setup:
- CCS: Version: 4.2.4.00033
- bios_6_32_02_39
- xdctools_3_22_01_21
I am porting some platform-agnostic framework/C-code from a C6472 platform to a C6424 platform and am seeing some problems... I have pared it down to a simple example - attached cfg and source file.
I am running these examples on the simulator and using the default RTSC platforms:
- ti.platforms.evm6472 (default speed = 700 MHz)
- ti.platforms.evm6424 (default speed = 594 MHz)
Given that the default tick is 1000us = 1 ms, the C6472 sim counts ~ 700k clocks, which is to be expected.
But, is the timer on C6424 running/updating @ ~ 1/2 clock rate? I did not find anything in the C6424 timer-peripheral spec to indicate that...
Calibrating/measuring timestamps is essential to our design.
Any help is greatly appreciated.
Thanks in advance!