Part Number: SK-AM62A-LP
Tool/software:
Hi TI,
I've been testing the AM62A board since last week.
First, I tried booting using tisdk-edgeai-image-am62axx-evm.wic.xz, the SD card image provided in TI-LINUX-SDK.
When using the image of SDK v10x(19 Aug 2024) and creating an SD card with balenaetcher,
all boot loader files (tiboo3.bin, tispl.bin, u-boot.img) are present in the boot folder,
but no message is displayed in the terminal. It appears that booting failed.
When using Linux-SDK v09x SD card image, it failed to boot normally, just like v10x.
This time, I unzipped xz and wrote it to the SD card using win32diskimager, and booting was successful.

However, if you write the SD card image of Linux-SDK v08x(27 Feb 2023) using balenaetcher,
it is confirmed that it boots normally.

i am using balenetcher v1.19.25
To successfully boot, first write Linux SDK v10x to the SD card.
Then, just overwrite tispl.bin of Linux SDK v08x on the SD card.
In other words, booting was possible just by replacing tispl.bin.
1) Is there a reason why only the v08x image boots normally when using balenaetcher?
2) Is there a mistake in failing to boot with the v10x image?
Thanks