Other Parts Discussed in Thread: TMS320C6747
Dear Sir:
Pls help me to answer below question. Thanks~
1. I want to run USB2.0 High speed slave mode at C6747. The software of USB2.0 (EX: USB stack....) is ready at C6747? Or I need to codeing USB 2.0?
2. When USB2.0 High speed slave mode at C6747 is running, C6747' performance will be hold and system can't run other code? How many performance will be reduced?
3. SDRAM is needed to mount at board? Can I mount DDR2? Can I just mount one 32bit SDRAMat board?
4. About Boot mode, Can I mount 2M bits SPI EEPROM where all code is inside?
5. What code size of USB 2.0 High speed slave mode is ? 2Mbit SPI EEPROM is enough?
6. The spec is shown GPIO, the GPIO can be input and output?
7.Pin USB_REFCLKIN is needed to connect to clock source? What frequence of clocj source is ?
8.The USB PHY needs 1.8V?
9.Pin number H4 and F3 is NC at spec, but they are VSS at circuit. Which name is right?
10. In instruction, is there instruction about Matrix rotate?
11. The code of SD/MMC is ready?
12. What security protection of user code can user use?