This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: SD Card detect pin- Hardware/software change requirements

Part Number: AM3358

Tool/software:

Hi TI Team,
In my current design with AM3358 I am using pin C15 as SD Card Detect and its working fine(AM3358 booting from SD card). Now for some additional functionality I need to use C15 as a UART pin and want to change MMC0_SDCD SD Card Detect pin to other pin of SD Card detect i.e A13 or M17, As these are the two other options available.

Will this hardware change requires any firmware/software change ? If yes, then what are the changes I need to do?