Tool/software:
Hi,
we are Configuring the Sdhci2 to connect an SD card as an Memory device to be detected in our yocto system.
below are the pin configurations
sdhci2: mmc@fa20000 {
compatible = "ti,am62-sdhci";
reg = <0x00 0x0fa20000 0x00 0x1000>, <0x00 0x0fa28000 0x00 0x400>;
interrupts = <GIC_SPI 82 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&k3_pds 184 TI_SCI_PD_EXCLUSIVE>;
clocks = <&k3_clks 184 5>, <&k3_clks 184 6>;
clock-names = "clk_ahb", "clk_xin";
bus-width = <4>;
ti,clkbuf-sel = <0x7>;
ti,otap-del-sel-legacy = <0x8>;
ti,otap-del-sel-sd-hs = <0x0>;
ti,otap-del-sel-sdr12 = <0x0>;
ti,otap-del-sel-sdr25 = <0x0>;
ti,otap-del-sel-sdr50 = <0x8>;
ti,otap-del-sel-sdr104 = <0x7>;
ti,otap-del-sel-ddr50 = <0x8>;
ti,itap-del-sel-legacy = <0xa>;
ti,itap-del-sel-sd-hs = <0xa>;
ti,itap-del-sel-sdr12 = <0xa>;
ti,itap-del-sel-sdr25 = <0x1>;
status = "disabled";
};
/* On-module Wi-Fi on WB SKUs, module-specific SDIO otherwise */
pinctrl_sdhci2: main-mmc2-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x120, PIN_INPUT, 0) /* (C24) MMC2_CMD */ /* WiFi_SDIO_CMD */
AM62X_IOPAD(0x118, PIN_INPUT, 0) /* (D25) MMC2_CLK */ /* WiFi_SDIO_CLK */
AM62X_IOPAD(0x114, PIN_INPUT, 0) /* (B24) MMC2_DAT0 */ /* WiFi_SDIO_DATA0 */
AM62X_IOPAD(0x110, PIN_INPUT, 0) /* (C25) MMC2_DAT1 */ /* WiFi_SDIO_DATA1 */
AM62X_IOPAD(0x10c, PIN_INPUT, 0) /* (E23) MMC2_DAT2 */ /* WiFi_SDIO_DATA2 */
AM62X_IOPAD(0x108, PIN_INPUT, 0) /* (D24) MMC2_DAT3 */ /* WiFi_SDIO_DATA3 */
AM62X_IOPAD(0x11c, PIN_INPUT, 0) /* (#N/A) MMC2_CLKB */
AM62X_IOPAD(0x0124, PIN_INPUT_PULLUP, 7) /* (A23) MMC2_SDCD.GPIO0_71 */
>;
};
/* MMC2 */
&sdhci2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sdhci2>;
cd-gpios = <&main_gpio0 71 GPIO_ACTIVE_LOW>;
disable-wp;
ti,driver-strength-ohm = <50>;
ti,fails-without-test-cd;
status = "okay";
};
Sd card is always powered with 3.3v and there is no witch to control the power.
the SD card we are using supports upto UHS class -1.

we are booting from the emmc using MMC0 and MMC1 is not used.
below are the boot logs:
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 6.1.80-6.7.0-devel+git.603f75dc931d (oe-user@oe-host) (aarch64-tdx-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Wed Aug 28 15:15:41 UTC 2024 [ 0.000000] Machine model: Toradex Verdin AM62 on Verdin Development Board [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000bfffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009dafffff] [ 0.000000] node 0: [mem 0x000000009db00000-0x000000009e6fffff] [ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff] [ 0.000000] node 0: [mem 0x000000009e780000-0x000000009fffffff] [ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000bfffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff] [ 0.000000] cma: Reserved 128 MiB at 0x00000000b6c00000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 20 pages/cpu s41064 r8192 d32664 u81920 [ 0.000000] pcpu-alloc: s41064 r8192 d32664 u81920 alloc=20*4096 [ 0.000000] pcpu-alloc: [0] 0 [0] 1 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] alternatives: applying boot alternatives [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 258048 [ 0.000000] Kernel command line: root=PARTUUID=acf35290-02 ro rootwait console=tty1 console=ttyS2,115200 consoleblank=0 earlycon=ns16550a,mmio32,0x02800000 [ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 840536K/1048576K available (11136K kernel code, 1360K rwdata, 3816K rodata, 2176K init, 424K bss, 76968K reserved, 131072K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 256 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GICv3: GICv3 features: 16 PPIs [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000080030000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000 [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention. [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008611] Console: colour dummy device 80x25 [ 0.013625] printk: console [tty1] enabled [ 0.017871] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.028565] pid_max: default: 32768 minimum: 301 [ 0.033342] LSM: Security Framework initializing [ 0.038210] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear) [ 0.045797] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear) [ 0.055762] cblist_init_generic: Setting adjustable number of callback queues. [ 0.063239] cblist_init_generic: Setting shift to 1 and lim to 1. [ 0.069546] cblist_init_generic: Setting adjustable number of callback queues. [ 0.076954] cblist_init_generic: Setting shift to 1 and lim to 1. [ 0.083353] rcu: Hierarchical SRCU implementation. [ 0.088271] rcu: Max phase no-delay instances is 1000. [ 0.094303] Platform MSI: msi-controller@1820000 domain created [ 0.100919] EFI services will not be available. [ 0.105890] smp: Bringing up secondary CPUs ... [ 0.111252] Detected VIPT I-cache on CPU1 [ 0.111379] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 0.111401] GICv3: CPU1: using allocated LPI pending table @0x0000000080050000 [ 0.111466] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.111593] smp: Brought up 1 node, 2 CPUs [ 0.141042] SMP: Total of 2 processors activated. [ 0.145863] CPU features: detected: 32-bit EL0 Support [ 0.151147] CPU features: detected: CRC32 instructions [ 0.156469] CPU: All CPU(s) started at EL2 [ 0.160663] alternatives: applying system-wide alternatives [ 0.168063] devtmpfs: initialized [ 0.180870] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.190921] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.203711] pinctrl core: initialized pinctrl subsystem [ 0.209916] DMI not present or invalid. [ 0.214584] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.221861] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations [ 0.229215] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.237226] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.245429] audit: initializing netlink subsys (disabled) [ 0.251235] audit: type=2000 audit(0.160:1): state=initialized audit_enabled=0 res=1 [ 0.251766] thermal_sys: Registered thermal governor 'step_wise' [ 0.259176] thermal_sys: Registered thermal governor 'power_allocator' [ 0.265540] cpuidle: using governor menu [ 0.276473] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.283484] ASID allocator initialised with 65536 entries [ 0.302978] KASLR disabled due to lack of seed [ 0.313871] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages [ 0.320868] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page [ 0.327288] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages [ 0.334236] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page [ 0.340651] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages [ 0.347598] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page [ 0.354012] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages [ 0.360958] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page [ 0.369068] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected [ 0.379267] iommu: Default domain type: Translated [ 0.384293] iommu: DMA domain TLB invalidation policy: strict mode [ 0.391016] SCSI subsystem initialized [ 0.395049] libata version 3.00 loaded. [ 0.395251] usbcore: registered new interface driver usbfs [ 0.400917] usbcore: registered new interface driver hub [ 0.406378] usbcore: registered new device driver usb [ 0.412030] pps_core: LinuxPPS API ver. 1 registered [ 0.417119] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.426480] PTP clock support registered [ 0.430630] EDAC MC: Ver: 3.0.0 [ 0.434953] FPGA manager framework [ 0.438560] Advanced Linux Sound Architecture Driver Initialized. [ 0.445864] clocksource: Switched to clocksource arch_sys_counter [ 0.452419] VFS: Disk quotas dquot_6.6.0 [ 0.456492] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.469636] NET: Registered PF_INET protocol family [ 0.474920] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.483638] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear) [ 0.492287] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.500235] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.508228] TCP bind hash table entries: 8192 (order: 6, 262144 bytes, linear) [ 0.515951] TCP: Hash tables configured (established 8192 bind 8192) [ 0.522658] UDP hash table entries: 512 (order: 2, 16384 bytes, linear) [ 0.529469] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear) [ 0.536887] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.543247] RPC: Registered named UNIX socket transport module. [ 0.549354] RPC: Registered udp transport module. [ 0.554172] RPC: Registered tcp transport module. [ 0.558987] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.565587] NET: Registered PF_XDP protocol family [ 0.571343] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.581534] Initialise system trusted keyrings [ 0.586429] workingset: timestamp_bits=46 max_order=18 bucket_order=0 [ 0.597555] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.604294] NFS: Registering the id_resolver key type [ 0.609547] Key type id_resolver registered [ 0.613832] Key type id_legacy registered [ 0.617996] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.624860] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.668426] Key type asymmetric registered [ 0.672634] Asymmetric key parser 'x509' registered [ 0.677692] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.685483] io scheduler mq-deadline registered [ 0.690130] io scheduler kyber registered [ 0.697822] pinctrl-single 4084000.pinctrl: 34 pins, size 136 [ 0.704612] pinctrl-single f4000.pinctrl: 171 pins, size 684 [ 0.716928] Serial: 8250/16550 driver, 8 ports, IRQ sharing enabled [ 0.734421] brd: module loaded [ 0.742552] loop: module loaded [ 0.749752] tun: Universal TUN/TAP device driver, 1.6 [ 0.755769] VFIO - User Level meta-driver version: 0.3 [ 0.761889] usbcore: registered new interface driver usb-storage [ 0.768697] i2c_dev: i2c /dev entries driver [ 0.775184] sdhci: Secure Digital Host Controller Interface driver [ 0.781572] sdhci: Copyright(c) Pierre Ossman [ 0.786276] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.792663] ledtrig-cpu: registered to indicate activity on CPUs [ 0.799009] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.805978] usbcore: registered new interface driver usbhid [ 0.811690] usbhid: USB HID core driver [ 0.816659] optee: probing for conduit method. [ 0.821278] optee: revision 3.20 (8e74d476) [ 0.821623] optee: dynamic shared memory is enabled [ 0.831193] optee: initialized driver [ 0.836964] Initializing XFRM netlink socket [ 0.841431] NET: Registered PF_PACKET protocol family [ 0.846707] Key type dns_resolver registered [ 0.851564] registered taskstats version 1 [ 0.855797] Loading compiled-in X.509 certificates [ 0.870304] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') [ 0.949292] i2c 0-0030: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/pmic@30/regulators/buck2 [ 0.990291] input: tps65219-pwrbutton as /devices/platform/bus@f0000/20000000.i2c/i2c-0/0-0030/tps65219-pwrbutton.2.auto/input/input0 [ 1.004635] rtc-ds1307 0-0032: oscillator failed, set time! [ 1.010548] rtc-ds1307 0-0032: registered as rtc0 [ 1.015514] rtc-ds1307 0-0032: hctosys: unable to read the hardware clock [ 1.024422] at24 0-0050: supply vcc not found, using dummy regulator [ 1.031426] at24 0-0050: 256 byte 24c02 EEPROM, writable, 16 bytes/write [ 1.038363] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz [ 1.070421] lm73 1-0049: sensor 'lm73' [ 1.075012] lm73 1-004a: sensor 'lm73' [ 1.078901] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz [ 1.084892] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created [ 1.093265] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created [ 1.102532] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created [ 1.113567] ti-udma 485c0100.dma-controller: Number of rings: 82 [ 1.121960] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18) [ 1.133128] ti-udma 485c0000.dma-controller: Number of rings: 150 [ 1.143445] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15) [ 1.153902] printk: console [ttyS2] disabled [ 1.158386] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 287, base_baud = 3000000) is a 8250 [ 1.167292] printk: console [ttyS2] enabled [ 1.175763] printk: bootconsole [ns16550a0] disabled [ 1.187060] 2810000.serial: ttyS0 at MMIO 0x2810000 (irq = 288, base_baud = 3000000) is a 8250 [ 1.196771] 2820000.serial: ttyS3 at MMIO 0x2820000 (irq = 289, base_baud = 3000000) is a 8250 [ 1.206531] 2830000.serial: ttyS5 at MMIO 0x2830000 (irq = 290, base_baud = 3000000) is a 8250 [ 1.216211] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 291, base_baud = 3000000) is a 8250 [ 1.225880] 2850000.serial: ttyS4 at MMIO 0x2850000 (irq = 292, base_baud = 3000000) is a 8250 [ 1.235498] 2860000.serial: ttyS7 at MMIO 0x2860000 (irq = 293, base_baud = 3000000) is a 8250 [ 1.245897] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode [ 1.289881] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.298711] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006 [ 1.311590] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5 [ 1.318730] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512 [ 1.325509] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0 [ 1.336155] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19 [ 1.346654] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller [ 1.352255] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 1 [ 1.360140] xhci-hcd xhci-hcd.3.auto: USB3 root hub has no ports [ 1.366154] xhci-hcd xhci-hcd.3.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000008020010010 [ 1.375612] xhci-hcd xhci-hcd.3.auto: irq 297, io mem 0x31000000 [ 1.382475] hub 1-0:1.0: USB hub found [ 1.386280] hub 1-0:1.0: 1 port detected [ 1.497912] mmc0: CQHCI version 5.10 [ 1.500366] gpio-427 (CTRL_SLEEP_MOCI#): hogged as output/high [ 1.516778] debugfs: Directory 'spi0.0' with parent 'regmap' already present! [ 1.524138] max310x spi0.0: MAX3109 ID 0xf3 does not match [ 1.531291] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode [ 1.542933] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit [ 1.577870] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.591401] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867 [ 1.601247] sdhci-am654 fa20000.mmc: Got CD GPIO [ 1.606592] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present! [ 1.606849] mmc2: CQHCI version 5.10 [ 1.617312] input: gpio-keys as /devices/platform/gpio-keys/input/input1 [ 1.627778] mmc0: new HS200 MMC card at address 0001 [ 1.633934] mmcblk0: mmc0:0001 Q2J55L 7.09 GiB [ 1.640844] mmcblk0: p1 p2 [ 1.642421] ALSA device list: [ 1.644652] mmcblk0boot0: mmc0:0001 Q2J55L 16.0 MiB [ 1.646833] No soundcards found. [ 1.653164] mmcblk0boot1: mmc0:0001 Q2J55L 16.0 MiB [ 1.659634] mmc2: SDHCI controller on fa20000.mmc [fa20000.mmc] using ADMA 64-bit [ 1.661284] mmcblk0rpmb: mmc0:0001 Q2J55L 4.00 MiB, chardev (241:0) [ 1.679973] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem [ 1.687376] EXT4-fs (mmcblk0p2): write access will be enabled during recovery [ 2.658396] EXT4-fs (mmcblk0p2): recovery complete [ 2.665085] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Quota mode: none. [ 2.673751] VFS: Mounted root (ext4 filesystem) readonly on device 179:2. [ 2.681388] devtmpfs: mounted [ 2.685994] Freeing unused kernel memory: 2176K [ 2.690644] Run /sbin/init as init process [ 2.694761] with arguments: [ 2.694768] /sbin/init [ 2.694774] with environment: [ 2.694779] HOME=/ [ 2.694785] TERM=linux [ 2.828619] systemd[1]: System time before build time, advancing clock. [ 2.875034] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid) [ 2.907105] systemd[1]: Detected architecture arm64. [ 2.972703] systemd[1]: Hostname set to <verdin-am62-15133535>. [ 3.317845] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6. [ 3.326865] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6. [ 3.415183] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6. [ 3.447291] systemd[1]: Queued start job for default target Graphical Interface. [ 3.510125] systemd[1]: Created slice Slice /system/getty. [ 3.536463] systemd[1]: Created slice Slice /system/modprobe. [ 3.560737] systemd[1]: Created slice Slice /system/serial-getty. [ 3.585708] systemd[1]: Created slice User and Session Slice. [ 3.599866] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ 3.622459] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ 3.646683] systemd[1]: Reached target Host and Network Name Lookups. [ 3.670098] systemd[1]: Reached target Path Units. [ 3.686192] systemd[1]: Reached target Remote File Systems. [ 3.706340] systemd[1]: Reached target Slice Units. [ 3.722312] systemd[1]: Reached target Swaps. [ 3.787808] systemd[1]: Listening on RPCbind Server Activation Socket. [ 3.810578] systemd[1]: Reached target RPC Port Mapper. [ 3.837176] systemd[1]: Listening on Syslog Socket. [ 3.855138] systemd[1]: Listening on initctl Compatibility Named Pipe. [ 3.880631] systemd[1]: Listening on Journal Audit Socket. [ 3.903848] systemd[1]: Listening on Journal Socket (/dev/log). [ 3.928136] systemd[1]: Listening on Journal Socket. [ 3.946240] systemd[1]: Listening on Network Service Netlink Socket. [ 3.973279] systemd[1]: Listening on udev Control Socket. [ 3.996266] systemd[1]: Listening on udev Kernel Socket. [ 4.020657] systemd[1]: Listening on User Database Manager Socket. [ 4.070731] systemd[1]: Mounting Huge Pages File System... [ 4.122711] systemd[1]: Mounting POSIX Message Queue File System... [ 4.156491] systemd[1]: Mounting Kernel Debug File System... [ 4.179503] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing). [ 4.204060] systemd[1]: Mounting Temporary Directory /tmp... [ 4.243057] systemd[1]: Starting Create List of Static Device Nodes... [ 4.277213] systemd[1]: Starting Load Kernel Module configfs... [ 4.323305] systemd[1]: Starting Load Kernel Module drm... [ 4.356483] systemd[1]: Starting Load Kernel Module fuse... [ 4.382758] fuse: init (API version 7.37) [ 4.407180] systemd[1]: Starting RPC Bind... [ 4.436153] systemd[1]: Starting File System Check on Root Device... [ 4.487176] systemd[1]: Starting Journal Service... [ 4.513502] systemd[1]: Starting Load Kernel Modules... [ 4.559667] systemd[1]: Starting Generate network units from Kernel command line... [ 4.592600] systemd[1]: Starting Coldplug All udev Devices... [ 4.627076] systemd[1]: Started RPC Bind. [ 4.647028] systemd[1]: Started Journal Service. [ 5.048609] EXT4-fs (mmcblk0p2): re-mounted. Quota mode: none. [ 5.183778] systemd-journald[156]: Received client request to flush runtime journal. [ 5.341343] audit: type=1334 audit(1651167747.508:2): prog-id=5 op=LOAD [ 5.351517] audit: type=1334 audit(1651167747.508:3): prog-id=6 op=LOAD [ 6.400210] ina2xx 1-0040: power monitor ina260 (Rshunt = 0 uOhm) [ 6.429925] random: crng init done [ 6.441075] ina2xx 1-0041: power monitor ina260 (Rshunt = 0 uOhm) [ 6.475961] ina2xx 1-0042: power monitor ina260 (Rshunt = 0 uOhm) [ 6.484625] ina2xx 1-0043: power monitor ina260 (Rshunt = 0 uOhm) [ 6.496279] omap8250 2b300000.serial: No clock speed specified: using default: 48000000 [ 6.509690] 2b300000.serial: ttyS1 at MMIO 0x2b300000 (irq = 482, base_baud = 3000000) is a 8250 [ 6.510847] ina2xx 1-0044: power monitor ina260 (Rshunt = 0 uOhm) [ 6.531810] ina2xx 1-0045: power monitor ina260 (Rshunt = 0 uOhm) [ 6.545575] ina2xx 1-0046: power monitor ina260 (Rshunt = 0 uOhm) [ 6.563935] ina2xx 1-0047: power monitor ina260 (Rshunt = 0 uOhm) [ 6.591277] ina2xx 1-004b: power monitor ina260 (Rshunt = 0 uOhm) [ 6.681439] pwm-backlight backlight-mezzanine: supply power not found, using dummy regulator [ 6.847367] k3-m4-rproc 5000000.m4fss: device does not reserved memory regions, ret = -22 [ 6.863877] k3-m4-rproc 5000000.m4fss: reserved memory init failed, ret = -22 [ 6.885781] remoteproc remoteproc0: releasing 5000000.m4fss [ 6.893088] k3-m4-rproc: probe of 5000000.m4fss failed with error -22 [ 6.962243] rtc-ti-k3 2b1f0000.rtc: registered as rtc1 [ 7.012734] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1) [ 7.037082] platform 78000000.r5f: configured R5F for IPC-only mode [ 7.063836] pvrsrvkm: loading out-of-tree module taints kernel. [ 7.089005] platform 78000000.r5f: device does not have reserved memory regions, ret = -22 [ 7.105369] k3_r5_rproc bus@f0000:bus@b00000:r5fss@78000000: reserved memory init failed, ret = -22 [ 7.115390] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0 [ 7.126536] remoteproc remoteproc0: releasing 78000000.r5f [ 7.138258] PVR_K: 183: Device: fd00000.gpu [ 7.138537] PVR_K: 183: Read BVNC 33.15.11.3 from HW device registers [ 7.138788] PVR_K: 183: RGX Device registered with BVNC 33.15.11.3 [ 7.139056] Console: switching to colour frame buffer device 240x67 [ 7.139939] [drm] Initialized pvr 23.3.6512818 20170530 for fd00000.gpu on minor 1 [ 7.216442] k3_r5_rproc bus@f0000:bus@b00000:r5fss@78000000: k3_r5_cluster_rproc_init failed, ret = -22 [ 7.216570] k3_r5_rproc: probe of bus@f0000:bus@b00000:r5fss@78000000 failed with error -22 [ 7.278042] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device [ 9.523485] remoteproc remoteproc0: 30074000.pru is available [ 9.533141] remoteproc remoteproc1: 30078000.pru is available [ 10.265616] audit: type=1334 audit(1651269009.024:4): prog-id=7 op=LOAD [ 10.274305] audit: type=1334 audit(1651269009.032:5): prog-id=8 op=LOAD [ 10.796941] audit: type=1334 audit(1651269009.556:6): prog-id=9 op=LOAD [ 10.808063] audit: type=1334 audit(1651269009.568:7): prog-id=10 op=LOAD [ 11.616757] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 11.653535] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 11.663585] cfg80211: Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600' [ 11.748962] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=356) [ 11.759346] audit: type=1334 audit(1651269010.520:8): prog-id=11 op=LOAD [ 11.771437] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode [ 11.773583] audit: type=1334 audit(1651269010.528:9): prog-id=12 op=LOAD [ 12.371684] audit: type=1334 audit(1651269011.132:10): prog-id=13 op=LOAD [ 12.379485] audit: type=1334 audit(1651269011.140:11): prog-id=14 op=LOAD [ 12.847445] audit: type=1006 audit(1651269011.608:12): pid=552 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1 [ 12.869274] audit: type=1300 audit(1651269011.608:12): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=fffff4e5af80 a2=1 a3=0 items=0 ppid=1 pid=552 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null) [ 12.895460] audit: type=1327 audit(1651269011.608:12): proctitle="(systemd)" [ 12.916309] audit: type=1334 audit(1651269011.676:13): prog-id=15 op=LOAD [ 13.777304] PVR_K: 546: RGX Firmware image 'rgx.fw.33.15.11.3' loaded [ 13.791561] PVR_K: 546: Shader binary image 'rgx.sh.33.15.11.3' loaded [ 13.813827] systemd-journald[156]: Data hash table of /run/log/journal/7557ee5ac0174e58b6c93fd1fc1934a2/system.journal has a fill level at 75.0 (2731 of 3640 items, 2097152 file size, 767 bytes per hash table item), suggesting rotation. [ 13.835196] systemd-journald[156]: /run/log/journal/7557ee5ac0174e58b6c93fd1fc1934a2/system.journal: Journal header limits reached or header out-of-date, rotating. [ 24.678880] TI DP83867 8000f00.mdio:00: Downshift occurred from negotiated speed 1Gbps to actual speed 100Mbps, check cabling! [ 24.690974] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx [ 24.779001] 8021q: 802.1Q VLAN Support v1.8 [ 24.783691] 8021q: adding VLAN 0 to HW filter on device eth0 [ 42.418245] kauditd_printk_skb: 10 callbacks suppressed [ 42.418285] audit: type=1334 audit(1651269041.180:18): prog-id=12 op=UNLOAD [ 42.430838] audit: type=1334 audit(1651269041.180:19): prog-id=11 op=UNLOAD