Other Parts Discussed in Thread: DM3730
We seem to be having a hard time finding X-loader code that still supports the DM3730 via UART3 (Serial Boot). We were hoping to use this method to initially get U-boot loaded into the NAND flash. Thus far, TimeSys and LogicPD don't really seem to have a solution. Can you check with TI to see if they might know where we can find a version of X-loader that will support serial boot on the DM3730? We would like to make sure we are not re-inventing the wheel prior to adding this functionality. I assume that U-boot can be written to NAND via a combination of a HW debugger and Debug software. -Tom-