I am trying to boot up with a RAMDISK file system. I get a kernel panic at boot. I'm not sure if the boot args are wrong or the filesystem image is wrong. I'm working with a DaVinci board. I can get the image into RAM just fine. In the past, I was successful in booting from the NAND. I would have thought the two procedures, RAMDISK vs NAND, were similar. I tried to use the ARAGO sample file system but it crashed at boot complaining about libs not being present. I tried using the file system which came with the EZSDK as the base of my RAMDISK file system. The resulting image was very large even after a gzip (80+M). Where can I find a per-built RAMDISK? This would test if my boot args or memory location assignment was wrong. I'm using the kernel image which came with EZSDK. Was it configured to handle RAMDISK file systems?