This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM35xx platform USB OTG cannot be change after Android boot up

Other Parts Discussed in Thread: AM3505

DEar Sir,

I built a android system base on Am3505 platform, but once I config the USB OTG as host when system boot up, then it is a host port only even I config to device, seems not successful until system reboot.

I expect USB OTG driver in android sytem is automatically detect the plug in device is a host product or slave product eg. if I plug a mouse to  the OTG port than it will become a host port or if I connect to PCB then this OTG port will become a slave port automatically. am I right?

BR

Edwin