Part Number: J784S4XEVM
Tool/software:
Is it possible to use the vlukan validation Layers on Jacinto? If yes how?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: J784S4XEVM
Tool/software:
Is it possible to use the vlukan validation Layers on Jacinto? If yes how?
Thanks, was after the operating system under test which has been answered.
Will loop in someone more familiar with Linux to address this.
Thanks,
kb
Hello,
To my knowledge Vulkan is not officially supported by our TISDK and is missing some key libraries. But yes, Vulkan is enabled in the default SDK GPU driver however, you need to rebuild your file-system in Yocto to get the required libraries. I would have to look into exactly how to enable in the Yocto build if you're looking for specific steps.
Thanks,
Sarabesh S.
Hello,
I am out of office. Please expect a delay in response.
Thanks,
Sarabesh S.
Closing since HW Accelerated Vulkan is now enabled in the SDK. A useful tool for debugging Vulkan® ICD Loaders and devices is vulkaninfo. This command, when run without any arguments will present a list of all supported devices, associated parameters, and supported extensions. This is on the latest 11.0.
For 10.x SDK you can enable vulkan by adding the following to your local.conf: DISTRO_FEATURES:append = " opencl vulkan"
IMAGE_INSTALL:append = "vulkan-headers-dev"
save and rebuild filesystem with yocto
Regards,
Sarabesh S.