Part Number: DRA821U
Other Parts Discussed in Thread: DRA821,
Tool/software:
Upon importing the downloaded IBIS model https://www.ti.com/lit/zip/sprm775 and importing into Altium 24.
- ERROR (line 25) - File_name 'J7200_DRA821_v0p1.ibs' contains an upper case character 'J'.
- ERROR (line 25) - File_name 'J7200_DRA821_v0p1.ibs' contains an upper case character 'D'.
- ERROR (line 25) - File_name 'J7200_DRA821_v0p1.ibs' contains an upper case character 'R'.
- ERROR (line 25) - File_name 'J7200_DRA821_v0p1.ibs' contains an upper case character 'A'.
Editing the File-name so all characters are lowercase and reimporting causes the following error.
- ERROR - Unable to find Package Model 'j7200_package' for Component 'J7200'
- Errors : 1
- Warnings: 95
- File Failed
In the file there is another Package Definition named j7vcl_package, would be ok to use that one as Package Model or other model should be used?