This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VP-Q1: PCIe Interface and Clock

Part Number: TDA4VP-Q1


Tool/software:

Hello Experts We need to use PCIe interface for TDA4VP-88. Both in RC and EP. 

Need clarifications on the following

1. SERDES0 , PCIe1  will be used as 1 x 4L

      a. Can we configure this SERDES0 as 2 x 2L

2. If SoC configured as Root complex do we need to supply the clock? Or it can be supplied internally by PLL.

3. If SoC configured as Endpoint do we need to supply the clock? or it can be supplied internally.

4. If clock has to be applied to which pins do we need to apply the clock? SERDES0_REFCLK_x or PCIE_REFCLK1_x_OUT ?

regards

Ratheesh