Tool/software:
Background of the Issue:sdk:ti-processor-sdk-linux-edgeai-am62axx-evm-09_02_00_05
The device tree allocates 1G of memory, but actually, when checked through commands, only 372M is available.
Device Tree file for k3-am62a7-sk.dts:
The display on the board shows that the memtotal
is only 372MB.
How can I configure the device tree to ensure that the full 1G of memory is displayed?