Part Number: LAUNCHXL-CC1352P
Other Parts Discussed in Thread: CC1352P7, LP-XDS110,
Tool/software:
I have been trying to flash my launchxl-cc1352p1 with the simple empty program, but it fails with the following error:
```
CS_DAP_0: Error connecting to the target: DAP Connection Error. This could be caused by the device having gone to low power mode. Try forcing an external reset.If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information.
```
CCS Theia does detect the board correctly. It also updated the firmware on xds110 the first time I tried flashing.
I have all the jumpers connected in the middle JTAG header and the power is set to XDS110 power.
Here is my system information
CCS Theia: 1.5.1
OS: Fedora Sway Atomic 40
I was initially trying to use the launchxl xds110 for flashing a beagleconnect freedom cc1352p7, but it was also failing with the same error.
Am I missing something?