This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Silverlight WEC7 BSP 2.0.



I was building some basic Silverlight OSDesigns and noticed the following:

I am using the Silverlight OSDESIGN template with the Sample Home Screen enabled, 800x480. No Compositor, No VRFB. Using WEC7 Update 3 with the 2.0.x BSP.

 

1. Built OSDESIGN and deployed to a 3530 platform with ES 3.1 silicon.

-it ran fine but was slow as expected as it was just using GDI.

Enabled PowerVR with SGX Core Revision 121. Set BSP_XRPLUGIN_OPENGL.and rebuilt.

-It ran and showed much faster response as expected.

2. I then tried doing the exact same on a 3730 platform with ES1.1 silicon.

-it also ran fine but was slow with just GDI. (but was faster than 3530 GDI only as cpu is faster).

Enabled PowerVR with SGX Core Revision 125. Set BSP_XRPLUGIN_OPENGL and rebuilt.

-When I deployed all I get is a black screen. Everything else seems to load fine and the rest appears to be running.

Just as a test I tried to select Core Rev 121 instead of 125 but I get a load error right away  on startup.

 

any ideas?