Part Number: AM625
Other Parts Discussed in Thread: AM62A7
Tool/software:
Hello,
We are trying to interface with the Ethernet registers in u-boot on the am62x and am62a starter kits. Attempting to access the registers while no ethernet cable is connected leads to a "Synchronous Abort" error which causes the som to reset. This is seen on booth the 62x and the 62a.
62x:
U-Boot SPL 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)') SPL initial stack usage: 13408 bytes Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 U-Boot SPL 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)') SPL initial stack usage: 1856 bytes Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted U-Boot 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000) SoC: AM62X SR1.0 GP Model: Texas Instruments AM625 SK EEPROM not available at 80, trying to read at 81 Board: AM62-SKEVM rev E2 DRAM: 2 GiB Core: 72 devices, 32 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial Out: serial Err: serial Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 => dhcp ethernet@8000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT ! am65_cpsw_nuss_port ethernet@8000000port@1: phy_startup failed am65_cpsw_nuss_port ethernet@8000000port@1: am65_cpsw_start end error => mii dump 3 1 "Synchronous Abort" handler, esr 0x02000000 elr: 0000000002ef9458 lr : 00000000808259ac (reloc) elr: 0000000081d0f458 lr : 00000000ff63b9ac x0 : 00000000fd5fa550 x1 : 0000000000000003 x2 : 00000000ffffffff x3 : 0000000000000001 x4 : 0000000081d0f458 x5 : 00000000fd6015e0 x6 : 0000000000000075 x7 : 0000000000000044 x8 : 0000000000000010 x9 : 0000000000000008 x10: 0000000000000001 x11: 0000000000000000 x12: 00000000ffffffff x13: 0000000000000000 x14: 00000000fd5e7820 x15: 0000000000000002 x16: 0000000081d0f458 x17: 0000000081d0cf98 x18: 00000000fd5f6d80 x19: 00000000fd5e6d68 x20: 0000000000000003 x21: 0000000000000001 x22: 0000000000000003 x23: 00000000fd5e6d68 x24: 0000000000000003 x25: 0000000000000000 x26: 0000000000000001 x27: 00000000ff6f4000 x28: 00000000fd615cd0 x29: 00000000fd5e6c70 Code: 00000000 00000000 81d0f288 00000000 (80c801d8) Resetting CPU ... resetting ...
62a:
U-Boot SPL 2024.04-00052-gd8cef0b37a8-dirty (Oct 23 2024 - 08:44:53 -0400) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 13568 bytes Trying to boot from MMC2 Authentication passed Authentication passed Authentication passed Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 U-Boot SPL 2024.04-00052-gd8cef0b37a8-dirty (Oct 23 2024 - 08:45:05 -0400) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') Trying to boot from MMC2 Authentication passed Authentication passed U-Boot 2024.04-00052-gd8cef0b37a8-dirty (Oct 23 2024 - 08:45:05 -0400) SoC: AM62AX SR1.0 HS-FS Model: Texas Instruments AM62A7 SK DRAM: 2 GiB (effective 4 GiB) Core: 87 devices, 30 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 => dhcp ethernet@8000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT ! am65_cpsw_nuss_port ethernet@8000000port@1: phy_startup failed am65_cpsw_nuss_port ethernet@8000000port@1: am65_cpsw_start end error => mii dump 3 1 "Synchronous Abort" handler, esr 0x96000010, far 0x8000f80 elr: 000000008086237c lr : 0000000080862378 (reloc) elr: 00000000fff3f37c lr : 00000000fff3f378 x0 : 0000000000085e2c x1 : 00000000000003e8 x2 : 00000000ffffffff x3 : 0000000000000001 x4 : 00000000fff3f4e8 x5 : 00000000fdea81e0 x6 : 0000000000000075 x7 : 0000000000000044 x8 : 0000000000000010 x9 : 0000000000000001 x10: 00000000fdebed38 x11: 00000000ffffffff x12: 0000000000000000 x13: 00000000fde890e0 x14: 00000000ffffffff x15: 00000000fdec0f61 x16: 00000000fff3f4e8 x17: 0000000000000000 x18: 00000000fde9cda0 x19: 0000000000085e2c x20: 0000000008000f00 x21: 0000000000000003 x22: 00000000fdea7f30 x23: 00000000fde88df8 x24: 0000000000000003 x25: 0000000000000000 x26: 0000000000000001 x27: 00000000fffe8000 x28: 00000000fdea8ef0 x29: 00000000fde88cb0 Code: aa0003f4 d2800000 940154c5 aa0003f3 (b9408280) Resetting CPU ... resetting ...
Is this a known issue, or a configuration problem? How would we go about addressing this issue?
Thank you,
Joshua Bourgeot